queued_spi_interrupt_b2b_transfer_slave#
Overview#
The queued_spi_interrupt_b2b_transfer examples show how to use QUEUEDSPI driver in interrupt way:
In this example we need two boards, one board is used as QUEUEDSPI master and another board is used as QUEUEDSPI slave. The file ‘queued_spi_interrupt_b2b_transfer_slave.c’ includes the QUEUEDSPI slave code. This example uses the transactional API in QUEUEDSPI driver.
QUEUEDSPI master sends/receives data to/from QUEUEDSPI slave in interrupt. (DSPI Slave uses interrupt to receive/send the data)