ele_crypto_generic_rsa#
Overview#
The ELE Crypto Generic Example project is a demonstration program that uses the MCUX SDK software to perform generic crypto operations usign plaintext key with EdgeLock Enclave (ELE).
Running the demo#
Example output on terminal:
EdgeLock Enclave secure Sub-System Driver Example:
*********** Load EdgeLock FW ****************************** EdgeLock FW loaded and authenticated successfully.
****************** Start RNG ****************** EdgeLock RNG Start success. EdgeLock RNG ready to use.
*********** Generic Crypto RSA keygen ********************* RSA Key-Pair generation. RSA Key-pair generated successfully.
*********** Generic Crypto RSA PKCS#1.5 Signature gen ***** RSA signature with input as digest generated successfully. RSA signature with input as message generated successfully.
*********** Generic Crypto RSA PSS Signature gen ********** RSA signature generated successfully.
*********** Generic Crypto RSA 2048 PKCS#1.5 Verify ******* RSA verify success
*********** Generic Crypto RSA 3072 PSS Verify ************ RSA verify success
*********** Generic Crypto RSA PKCS#1.5 encrypt *********** RSA encryption success.
*********** Generic Crypto RSA PKCS#1.5 decrypt *********** RSA decryption success, plaintext match original one.
*********** Generic Crypto RSA OAEP encrypt *************** RSA encryption success.
*********** Generic Crypto RSA OAEP decrypt *************** RSA decryption success, plaintext match original one.
End of Example with SUCCESS!!