ele_hseb_demo#
Overview#
The ELE HSEB demo project is a demonstration program that uses the MCUX SDK software to perform crypto operations with HSEB EdgeLock Enclave (ELE) and usage of its services with direct use of Messaging Unit driver.
Running the demo#
Example output on terminal:
* ELE_HSEB Demo started *
Check if HSEB FW is installed...HSEB FW is installed
Get FW version...Sucess
Check if NVM and RAM key catalogs are formatted...Key catalogs are formatted
Import symmetric keys for cryptographic operation...Success
Try erase keys...Success
Check if NVM and RAM key catalogs are formatted...Key catalogs are not formatted
Formatting key catalogs...Success
Import symmetric keys for cryptographic operation...Success
Exercise crypto operations:
AES crypto - passed
HASH crypto - passed
Session key - passed
Sys authorization - passed
NVM key update - passed
AES get key info - passed
RSA crypto - passed
AEAD crypto - passed
All tests passed!!
Demo end
Supported Boards#
FRDM-MCXE31B
Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
ELE HSEB Firmware Installation Guide
Before using ELE HSEB, you must first install the ELE HSEB Firmware to your device.
For detailed instructions on firmware installation, please refer to the firmware
README file.
The relative path points to the edgelock firmware release repository that should
be available in your SDK at <sdk-root>/firmware/edgelock/.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
FRDM-MCXE32B
Hardware requirements
Type-C USB cable
FRDM-MCXE32B board
Personal Computer
Board settings
ELE HSEB Firmware Installation Guide
Before using ELE HSEB, you must first install the ELE HSEB Firmware to your device.
For detailed instructions on firmware installation, please refer to the firmware
README file.
The relative path points to the edgelock firmware release repository that should
be available in your SDK at <sdk-root>/firmware/edgelock/.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.