MCUXpresso SDK Documentation

ezhv_flexio_dvp

ezhv_flexio_dvp#

Overview#

This project shows how to use EZHV and FlexIO to enable display video port.

Supported Boards#

MIMXRT700-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

  • RK055AHD091 MIPI panel (Not necessary if use other panel)

  • RK055MHD091 MIPI panel (Not necessary if use other panel)

  • OV7670 module

Board settings

To use MIPI panel: Connect MIPI panel to J52.

Prepare the Demo

The demo use MIPI RK055MHD091 panel by default, to use MIPI RK055AHD091 panel, change the macro DEMO_PANEL to 0 in mcux_config.h.

  1. Connect a micro USB cable between the PC host and the USB port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo CM33
When the demo runs successfully, you will find the video is dislayed on the  
panel of RK055AHD091 or RK055MHD091.
and the terminal will display the following:
    EZH-V flexIO DVP example started
    Frame Update Rate: 28 fps
    Frame Update Rate: 28 fps
Note:

Connect the OV7670 camera sensor to J53 connector short 2-3 for JP7

Note:

If the camera frame buffer is placed in SRAM P18~P29, and camera resolution is set to 640x480, the EZHV firmware doesn’t work at 30Hz frame rate, 15Hz frame rate works. Root cause is accessing to these RAM_ARBITER1 partitions needs more clock cycles, so the EZHV can’t write camera data to the buffers in time.

FRDM-IMXRT700
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT700 board

  • Personal Computer

  • RaspberryPi Panel

  • OV7670 module

Board settings

JP7 2-3 connected. To use Raspberry panel: Connect the panel to J8. Then connect the panel’s 5V pin to JP43-1, GND pin to JP43-2.

Prepare the Demo

The demo use MIPI RaspberryPi panel by default.

  1. Connect a USB cable between the PC host and the USB port on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo CM33
When the demo runs successfully, you will find the video is dislayed on the  
panel.
and the terminal will display the following:
    EZH-V flexIO DVP example started
    Frame Update Rate: 28 fps
    Frame Update Rate: 28 fps
Note:

Connect the OV7670 camera sensor to J53 connector short 2-3 for JP7

Note:

If the camera frame buffer is placed in SRAM P18~P29, and camera resolution is set to 640x480, the EZHV firmware doesn’t work at 30Hz frame rate, 15Hz frame rate works. Root cause is accessing to these RAM_ARBITER1 partitions needs more clock cycles, so the EZHV can’t write camera data to the buffers in time.