MCUXpresso SDK Documentation

fmstr_example_can

fmstr_example_can#

Overview#

Example application demonstrates CAN bus communication. This requires a suitable CAN interface connected to the computer and interconnected with the target MCU using a properly terminated CAN bus. The typical transmission speed is 500 kbps. A FreeMASTER-over-CAN communication plug-in must be used.

Supported Boards#