MCUXpresso SDK Documentation

littlefs_shell

littlefs_shell#

Overview#

The littlefs_shell demonstrates the capabilities of LittleFS FLASH filesystem:

After the example is loaded into the target and launched the shell prompt is printed to the console. Type “help” to obtain list of available commands. The FLASH storage has to be formatted upon first use. After mounting the filesystem it is possible to create/delete/list directories and read/write files using appropriate commands. There is no concept of current directory in LittleFS, hence it is always necessary to specify full directory path.

List of supported commands: format Formats the filesystem mount Mounts the filesystem unmount Unmounts the filesystem ls Lists directory content rm Removes file or directory mkdir Creates a new directory write Writes/appends text to a file cat Prints file content

Example workflow: To perform initial format of the storage, issue ‘format yes’ command. Mount the storage by issuing ‘mount’ command. Create new directory by ‘mkdir mynewdir’. Create new file in the ‘mynewdir’ directory by writing line of text to it using ‘write mynewdir/foo.txt firstline’ Append another line to the same file using ‘write mynewdir/foo.txt secondline’ Print the content of the file using ‘cat mynewdir/foo.txt’. The expected output is: firstline secondline

Supported Boards#

EVKB-IMXRT1050
Hardware requirements
  • Mini/micro USB cable

  • EVKB-IMXRT1050 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

Note: LittleFS example built using arm-gcc does not work as expected out-of-the box. Other supported toolchains are not affected.

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
Copyright  2017  NXP
LFS>>
MIMXRT1060-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKB board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2018 NXP
LFS>>
MIMXRT1060-EVKC
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1060-EVKC board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
FRDM-IMXRT1152
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1152 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2026 NXP
LFS>>
EVK-MIMXRT1020
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1020-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MIMXRT1024-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1024-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MIMXRT1040-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1040-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
EVK-MIMXRT1064
Hardware requirements
  • Mini/micro USB cable

  • EVK-MIMXRT1064 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2018 NXP
LFS>>
MIMXRT1160-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1160-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

 * Copyright 2022 NXP
LFS>>
FRDM-MCXN947
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
FRDM-RW612
Hardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port (J10) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2018 NXP
LFS>>
LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:

  1. Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”

      This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
    
  2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):

    a. Open SEGGER J-FLASH Lite, select device LPC54S018.

    b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)

    c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
    The log below shows example output of the eeprom example in the terminal window:

SHELL (build: Feb 28 2018)
Copyright  2017  NXP
LFS>>
LPCXpresso55S36
Hardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

Board settings

IMPORTANT: Connect pin 2-3 of JP1 and JP56 (sets VCC_1V9 for MCU and flash) Connect pin 1-2 of JP41,JP42,JP43,JP44,JP45,JP64 and JP65. Close JP63, JP66,JP67,JP68 and JP69.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MCX-N5XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N5XX-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2021 NXP
LFS>>
MIMXRT700-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

Copyright 2024 NXP
LFS>>
FRDM-IMXRT700
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT700 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

Copyright 2024 NXP
LFS>>
RD-RW612-BGA
Hardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

SHELL (build: Feb 28 2018)
 * Copyright 2018 NXP
LFS>>
FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

 * Copyright 2022 NXP
LFS>>