lwip_httpssrv_mbedTLS_enet_qos_freertos#
Overview#
The lwip_httpsrv_mbedTLS demo application demonstrates an HTTP server set up on lwIP TCP/IP and the MbedTLS stack with FreeRTOS. The user uses an Internet browser to send an https request for connection. The board acts as an HTTP server and sends a web page back to the PC.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
MIMXRT1170-EVKB board
Personal Computer
Board settings
No special settings are required.