MCUboot and ota examples changelog#
All notable changes to MCUboot fork in MCUXpresso SDK and related ota examples will be documented in this file.
[26.09.0] - 09/2026#
Added#
Added basic support for FRDM-IMXRT1152 and FRDM-IMXRT700 boards
Changed#
Changed partition layouts on FRDM-MCXN266 and FRDM-MCXA336
Fixed#
(Encrypted XIP)(IPED) Fixed the reset issue during wifi initialization when IPED encryption is active
(MCXA266/MCXA366) Added flash access and MBC configuration to mcuboot startup to fix issues with flash operations during OTA if CMPA is present
[26.06.0] - 06/2026#
Added#
Encrypted XIP: Added experimental FLASH_REMAP mode (see Encrypted XIP doc)
Added basic support for FRDM-MCXC162 board
Changed#
Optimized PSA configuration for mcuboot_opensource to reduce binary size
(Encrypted XIP) Moved IPED dependencies in MCUBoot loader code to flash backend and reworked the extension
(Encrypted XIP) Documentation updated
[26.03.0] - 03/2026#
Added#
MCUboot updated to v2.3.0
Enabled ota_rom_basic for FRDM-MCXN236
Added new upgrade mode SINGLE_APPLICATION_SLOT
Enabled serial recovery feature (see Serial Recovery doc)
Changed#
Update Mbed TLS to 3.0 in ota_mcuboot_client example
Specify terminology of upgrade modes supported in ota examples with MCUBoot (see README)
FRDM-MCXA153 configured to use SINGLE_APPLICATION_SLOT mode due to its very limited flash size
LPCXpresso55S69 configured to use TinyCrypt due to higher flash usage of the latest mcuboot+mbedtls. Original prj.conf is left for reference.
[25.12.0] - 12/2025#
Added#
Added basic support for KW47-EVK and MCX-W72-EVK board
Added SB3 processing support for MIMXRT700EVK (see SB3 doc)
[25.09.0] - 09/2025#
Fixed#
(Encrypted XIP)(IPED) Fixed issue between IPED and PKC
Added#
Added new doc Kconfig and customization of OTA examples
Changed#
Update MCUboot to 2.2.0
Update Mbed TLS to 3.0 in mcuboot_opensource example
PSA Crypto API (MCUBOOT_USE_PSA_CRYPTO) is used in default configurations to utilize hardware acceleration
Legacy API (MCUBOOT_USE_MBED_TLS) is used in configuration using Encrypted XIP due limitations in PSA Crypto API in current MCUboot version
EC256 made as default signature algorithm replacing obsolete RSA
it is still possible to manually setup RSA but only for legacy API
Encrypted XIP: reworked the layer to use only the overwrite mode
Changed default partition layout on FRDM-RW612, RD-RW612BGA and EVKCMIMXRT1060:
mcuboot_opensource: 256kB
application: 2MB
Removed#
Encrypted XIP: removed the experimental three-slot mode
[25.06.0] - 06/2025#
Added#
Added
ota_rom_basicexample demonstrating ROM bootloader processing a secure binary as an OTA image (see documentation in docs folder)Enabled
ota_rom_basicexample for FRDM-MCXN947, MCX-N9XX-EVK, FRDM-RW612 and RD-RW612BGAEnabled flash remap feature for MIMXRT700EVK
FRDM-MCXE247 basic MCUboot support
FRDM-MCXN947, MCX-N5XX-EVK and MCX-N9XX-EVK supports alternative build using MCUboot located in the internal flash instead of the IFR region (default) - see board specific readme for more information
Removed#
Removed
ota_rom_server(replaced by simplerota_rom_basic)
[25.03.0] - 03/2025#
Added#
(MCXA20) Basic support for FRDM-MCXA276 and FRDM-MCXA166
Added SB3 processing support in
ota_mcuboot_basicexample for selected platforms(MCXN)(RW61x) Enabled SB3 processing support for FRDM-MCXN947, MCXN9XXEVK, FRDM-RW612 and RD-RW612BGA
Changed#
Update MCUboot to 2.1.0
Fixed#
(Encrypted XIP)(IPED) Fixed issues in wifi based examples using IPED encryption
(Encrypted XIP) Fixed missing default encryption keys
Removed#
Removed support for MDK toolchain
[24.12.0] - 12/2024#
Added#
Initial release
Removed#
Removed WiFi OTA examples on boards that also support Ethernet