MCUXpresso SDK Documentation

ota_rom_basic#

Overview#

This ota_rom_basic example demonstrates a basic application that uses ROM as a first stage bootloader. A secure binary (SB) is used as an image for OTA update.

Prepare the Demo#

  1. The demo requires provisioned device to function properly. Please refer to respective readme for your target board referenced in sb3_common_readme.md located in docs folder and follow the steps there before you continue.

  2. Connect a USB cable between the PC and the Debug USB port on the target board.

  3. Open a serial terminal on PC for connected board with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

    • Unix line ending using \n (LF)

Transfering data to the flash memory#

There are multiple ways how to transfer image updates to the flash memory:

  • This examples implements a simple XMODEM-CRC protocol, that can be used to transfer data to the board at slow speed (~10kB/s). This provides a convenient method for images that have relatively small size (under lower 100’s of kB). In the application shell the XMODEM receiving is initiated by xmodem_sb3 command. Terminal emulators like Tera Term or ExtraPutty can be used as a transmitting side. Both 128B and 1024B packet sizes are supported.

  • An alternative way, more suitable for larger images, is to use the blhost utility (part of NXP’s SPSDK and MCUXpresso Secure Provisioning Tool). Blhost communicates with chip’s ROM and supports all basic flash operations. When used via onboard’s USB the transfer speed is more appropriate for larger files. See board’s user manual for details on ISP mode.

  • Another option is to use a debug adapter (e.g. JLink, CMSIS DAP…) and flash data using their tools.

Running the demo#

To get the application properly executed by the ROM bootloader, it is necessary to put signed application image to the image region partition. There are multiple options how to achieve that, however in principle the are two main methods (both presuming the device is correctly provisioned):

  1. programing signed application image to the primary application partition using an external tool (direct method)

  2. jump-starting the application by debugger, performing an image update with the signed image, resetting the board and letting the bootloader to perform the update (indirect method)

The latter method is used in the following step-by-step description:

  1. Open the demo project and build it.

  2. Prepare SB file of the application from raw binary as described in the sb3_[&device]_readme.md for you board.

  3. Launch the debugger in your IDE to jump-start the application.

  4. When the demo starts successfully, the terminal will display shell prompt as in the following example:

    *************************************
    *  Basic ROM application example    *
    *************************************
    
    Built Feb 22 2025 14:09:14
    
    $
    
  5. Available commands can be printed with help command

  6. Current image state is printed with image command. The output will reflect settings of the used platform and may not be exactly the same as the following output:

    $ image
    IMAGE 0: Invalid image header 
    IMAGE 1: Invalid image header   	
    
  7. From the shown image command output it can be observed that there are currently no signed images present neither in the image 0 nor image 1 region. Since the example was started by a debugger, it is not signed and hence not recognized as a valid signed image in the image 0 region.

  8. XMODEM transfer is initiated using xmodem_sb3 command. When executed, it starts waiting for the transmitting side. In this demonstration Tera Term is used to send the update file. The dialog File->Transfer->XMODEM is used to select a file to be send. In the same dialog a packet size can be extended to 1kB for faster transmittion.

    $ xmodem_sb3
    Initiated XMODEM-CRC transfer. Receiving... (Press 'x' to cancel)
    CCC
    Received 41984 bytes
    SB3 has been processed
    
  9. After image downloaded finished the current image status can be checked with image command. The output now shows that there is an image file detected in the image 1 region.

    $ image
    IMAGE 0:Invalid image header 
    IMAGE 1:
    	<IMG_VERSION 0x1 LENGTH 34356 EXEC_ADDR 0x8001000>
    
  10. Running reboot command or resetting the board manually starts the bootloader and lets it handle the installation of new image. If everything went well the image in the image 1 region is validated and marked for boot. The image command output should reflect this change:

    $ image
    IMAGE 0:Invalid image header 
    IMAGE 1:
    	<IMG_VERSION 0x1 LENGTH 34356 EXEC_ADDR 0x8001000>
    	*ACTIVE*
    

Supported Boards#

FRDM-MCXN236
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • FRDM-MCXN236 board

  • Personal Computer

Board settings
Board provisioning details

For board provisioning it’s best to use MCUXpresso Secure Provisioning tool. Besides required setup the following settings need to be applied: - Boot type set as “Signed” - CFPA_PAGE_VERSION set to at least 1 (non-zero and non-all-one) - Flash swapping enabled; CMPA field FLASH_CFG.FLASH_REMAP_SIZE set to 0b11111

The Dual image boot option allows to select for which slot (slot0/slot1) the SB3 file is being created. To create SB3 file used for an update, the target image should be set as “Image 1” - this reflects the process of using the second dormant slot as a space for the new image. It’s important to realize that with Flash Swapping enabled the ROM selects an image with higher Image version. If higher version image is located in the second slot (offset 0x100000) it swaps the slot0/slot1 addresses making it effectively appear at the beginning of the flash (offset 0). Therefore also make sure that Image version of the new image is higher than the currently installed one.

For step-by-step walktrough look to sb3_common_readme.md located docs folder.

MIMXRT700-EVK
Hardware requirements
  • micro USB cable

  • MIMXRT700 board

  • Personal Computer

Board settings

No special HW settings.

Board provisioning details

For step-by-step walktrough look to sb3_common_readme.md located in docs folder.

FRDM-RW612
Hardware requirements
  • micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings

No special HW settings.

Board provisioning details

For step-by-step walktrough look to sb3_common_readme.md located in docs folder.

RD-RW612-BGA
Hardware requirements
  • micro USB cable

  • RDRW612BGA board

  • Personal Computer

Board settings
Board provisioning details

For step-by-step walktrough look to sb3_common_readme.md located in docs folder.

FRDM-MCXN947
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings
Board provisioning details

For board provisioning it’s best to use MCUXpresso Secure Provisioning tool. Besides required setup the following settings need to be applied: - Boot type set as “Signed” - CFPA_PAGE_VERSION set to at least 1 (non-zero and non-all-one) - Flash swapping enabled; CMPA field FLASH_CFG.FLASH_REMAP_SIZE set to 0b11111

The Dual image boot option allows to select for which slot (slot0/slot1) the SB3 file is being created. To create SB3 file used for an update, the target image should be set as “Image 1” - this reflects the process of using the second dormant slot as a space for the new image. It’s important to realize that with Flash Swapping enabled the ROM selects an image with higher Image version. If higher version image is located in the second slot (offset 0x100000) it swaps the slot0/slot1 addresses making it effectively appear at the beginning of the flash (offset 0). Therefore also make sure that Image version of the new image is higher than the currently installed one.

For step-by-step walktrough look to sb3_common_readme.md located docs folder.

FRDM-MCXN947T
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • FRDM-MCXN947T board

  • Personal Computer

Board settings
Board provisioning details

For board provisioning it’s best to use MCUXpresso Secure Provisioning tool. Besides required setup the following settings need to be applied: - Boot type set as “Signed” - CFPA_PAGE_VERSION set to at least 1 (non-zero and non-all-one) - Flash swapping enabled; CMPA field FLASH_CFG.FLASH_REMAP_SIZE set to 0b11111

The Dual image boot option allows to select for which slot (slot0/slot1) the SB3 file is being created. To create SB3 file used for an update, the target image should be set as “Image 1” - this reflects the process of using the second dormant slot as a space for the new image. It’s important to realize that with Flash Swapping enabled the ROM selects an image with higher Image version. If higher version image is located in the second slot (offset 0x100000) it swaps the slot0/slot1 addresses making it effectively appear at the beginning of the flash (offset 0). Therefore also make sure that Image version of the new image is higher than the currently installed one.

For step-by-step walktrough look to sb3_common_readme.md located docs folder.

MCX-N9XX-EVK
Hardware requirements
  • Mini/micro USB cable

  • RJ45 Network cable

  • MCX-N9XX-EVK board

  • Personal Computer

Board settings
Board provisioning details

For board provisioning it’s best to use MCUXpresso Secure Provisioning tool. Besides required setup the following settings need to be applied: - Boot type set as “Signed” - CFPA_PAGE_VERSION set to at least 1 (non-zero and non-all-one) - Flash swapping enabled; CMPA field FLASH_CFG.FLASH_REMAP_SIZE set to 0b11111

The Dual image boot option allows to select for which slot (slot0/slot1) the SB3 file is being created. To create SB3 file used for an update, the target image should be set as “Image 1” - this reflects the process of using the second dormant slot as a space for the new image. It’s important to realize that with Flash Swapping enabled the ROM selects an image with higher Image version. If higher version image is located in the second slot (offset 0x100000) it swaps the slot0/slot1 addresses making it effectively appear at the beginning of the flash (offset 0). Therefore also make sure that Image version of the new image is higher than the currently installed one.

For step-by-step walktrough look to sb3_common_readme.md located docs folder.