sgi_pkc_asymmetric#
Overview#
The SGI PKC application provides examples which demonstrate usage of most available algorithms and a crypto library lightweight testing:
AES-128 encryption/decryption, modes ECB/CBC/CTR/GCM/CMAC
SHA2-224/256/384/512 (including sha-direct mode)
ECC Sign/Verify/Keygen/Keyexchange
Supported Boards#
FRDM-MCXL255
Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI PKC asymmetric cipher example
============================
ECC ECDH key agreement NIST P256:pass
ECC ECDSA NIST P256:pass
RSA key generation:pass
ECC EdDSA verify signature Ed25519:pass
ECC MontDH Curve25519:pass
ECC MontDH Curve448:pass
ECC EdDSA Ed25519:pass
============================
RESULT: All 7 test PASS!!
ELS example END
FRDM-MCXA577
Hardware requirements
Type-C USB cable
FRDM-MCXA577 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI PKC asymmetric cipher example
============================
ECC ECDH key agreement NIST P256:pass
ECC ECDSA NIST P256:pass
RSA key generation:pass
ECC EdDSA verify signature Ed25519:pass
ECC MontDH Curve25519:pass
ECC MontDH Curve448:pass
ECC EdDSA Ed25519:pass
============================
RESULT: All 7 test PASS!!
SGI example END
FRDM-MCXA287
Hardware requirements
Type-C USB cable
FRDM-MCXA287 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI PKC asymmetric cipher example
============================
ECC ECDH key agreement NIST P256:pass
ECC ECDSA NIST P256:pass
RSA key generation:pass
ECC EdDSA verify signature Ed25519:pass
ECC MontDH Curve25519:pass
ECC MontDH Curve448:pass
ECC EdDSA Ed25519:pass
============================
RESULT: All 7 test PASS!!
SGI example END
FRDM-KW43
Hardware requirements
Type-C USB cable
FRDM-KW43 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI PKC asymmetric cipher example
============================
ECC ECDH key agreement NIST P256:pass
ECC ECDSA NIST P256:pass
RSA key generation:pass
ECC EdDSA verify signature Ed25519:pass
ECC MontDH Curve25519:pass
ECC MontDH Curve448:pass
ECC EdDSA Ed25519:pass
============================
RESULT: All 7 test PASS!!
SGI PKC example END
FRDM-MCXA266
Hardware requirements
Type-C USB cable
FRDM-MCXA266 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI PKC asymmetric cipher example
============================
ECC ECDH key agreement NIST P256:pass
ECC ECDSA NIST P256:pass
RSA key generation:pass
ECC EdDSA verify signature Ed25519:pass
ECC MontDH Curve25519:pass
ECC MontDH Curve448:pass
ECC EdDSA Ed25519:pass
============================
RESULT: All 7 test PASS!!
SGI PKC example END
FRDM-MCXA366
Hardware requirements
Type-C USB cable
FRDM-MCXA366 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
SGI PKC asymmetric cipher example
============================
ECC ECDH key agreement NIST P256:pass
ECC ECDSA NIST P256:pass
RSA key generation:pass
ECC EdDSA verify signature Ed25519:pass
ECC MontDH Curve25519:pass
ECC MontDH Curve448:pass
ECC EdDSA Ed25519:pass
============================
RESULT: All 7 test PASS!!
ELS example END