usb_pd_source_charger
Overview
The PD charger example is a simple demonstration based on the MCUXpresso SDK PD stack.
The application simulate charger product.
The demo only works as source and is external powered.
System Requirement
Hardware requirements
One or two Type-C shield board
One or two 9V DC power suppliers
Type-C Cable
One or two hardwares (Tower module/base board, and so on) for a specific device, for example: lpcxpresso54114 board
Personal Computer
Software requirements
The project files are in:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_pd_source_charger/ / .
The
is Bare Metal or FreeRTOS OS.
Terminal tool.
Getting Started
Hardware Settings
For detailed instructions, see the appropriate board User’s Guide.
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Download the program to the target board.
Power on Type-C shield board then power on development board.
Run the example
Connect the OpenSDA USB port to the PC and open terminal.
This charger provide power 5V/2.7A and 9V/1.5A.
Connect the sink with Type-C cable to the board, The board will print the sink’s request power information.
For example: Download usb_pd_charger_battery or usb_pd_sink_battery demo to another board and connect to the tested board.
Supported Boards
LPCXpresso55S69