MCUXpresso SDK Documentation

SDK Architecture Overview#

The MCUXpresso SDK uses a modular architecture where software components are distributed across multiple repositories hosted on GitHub and managed through the west tool. This approach provides flexibility, maintainability, and enables selective component inclusion.

Repository Organization#

Based on the manifest structure, the SDK consists of four main repository categories:

Manifest Repository#

The manifest repo (mcuxsdk-manifests) contains the west.yml manifest file that tracks all other repositories in the SDK.

Base Repositories#

Recorded in submanifests/base.yml and loaded in the root west.yml manifest file. These are the foundational repositories that build the SDK:

  • Devices: MCU-specific support packages

  • Examples: Demonstration applications and code samples

  • Boards: Board support packages

Middleware Repositories#

Recorded in the submanifests/middleware subdirectory, categorized according to functionality:

  • Connectivity: Networking stacks, USB, and communication protocols

  • Security: Cryptographic libraries and secure boot components

  • Wireless: Bluetooth, IEEE 802.15.4, and other wireless protocols

  • Graphics: Display drivers and UI frameworks

  • Audio: Audio processing and voice recognition libraries

  • Machine Learning: AI inference engines and neural network libraries

  • Safety: IEC60730B safety libraries

  • Motor Control: Motor control and real-time control libraries

Internal Repositories#

Recorded in submanifests/internal.yml and grouped into the “bifrost” group. These are only visible to NXP internal developers and hosted on NXP internal git servers.

Repository Hosting#

Public repositories are hosted on GitHub under these organizations:

Internal repositories are hosted on NXP’s private Git infrastructure.

Benefits of This Architecture#

Selective Integration: Projects include only required components, reducing memory footprint and build complexity.

Independent Versioning: Each component maintains its own release cycle and version control.

Community Collaboration: Public repositories accept community contributions through standard Git workflows.

Scalable Maintenance: Component owners can update their repositories without affecting the entire SDK.

Workspace Management#

The west tool manages repository synchronization, version tracking, and workspace updates. All repositories are checked out under the mcuxsdk/ directory with their designated paths defined in the manifest files.