Integration test#
A correct integration of the SSRC module can be verified in two ways.
Bit accurate test#
The TestFiles directory of the release package contains a test input (sampled at 44,100 Hz) and several expected output files (sample rates from 8000 Hz to 48,000 Hz). If the same test input file is applied to the SRC after integration in the target platform, the output is bit accurate with the expected output file that matches the output-sample rate
Parent topic:Integration test
THD+N measurement#
Produce a swept sine and feed it through the SSRC module. Do a THD+N measurement on the obtained output signal. The THD+N of the converted signals should be below - 77 in the interval [0 - 0.45] FsLOW.
Parent topic:Integration test