This document explains feature guards macros to be used during the transition from legacy to PSA in order to determine whether a given cryptographic mechanism is available in the current build.
We currently (as of Mbed TLS 3.6) have three sets of feature macros:
PSA_WANTmacros;legacy
MBEDTLS_xxxmacros;transitional
MBEDTLS_xxxmacros that stem from the desire to be able to use crypto mechanisms that are only provided by a driver (G5 instrategy.md).
This document’s goal is to shed some light on when to use which. It is mostly intended for maintainers.
Since most transition macros come from driver-only work, it can be useful to
check docs/driver-only-builds.md as well for background. (Note: as
maintainers, for the best precision about what’s supported of not with
drivers, check the relevant component_test_psa_crypto_config_accel_xxx’s
configuration, as well as the corresponding exclude list in
analyze_outcomes.py.)
General considerations#
This document only applies to Mbed TLS 3.6 TLS. By contrast:
in 2.28 we have no driver-only support, so the legacy guards
MBEDTLS_XXXshould be used everywhere;in 4.0 configuration will be purely based on PSA, so
PSA_WANTmacros should be used everywhere.
It is useful to consider the following domains:
The PSA domain: things declared in
include/psa/*.h, implemented inlibrary/psa_*.cand tested intests/suites/test_suite_psa*.The pure TLS 1.3 domain: the parts of TLS 1.3 that are not in the
USE_PSAdomain (see below). Those use PSA APIs unconditionally.The
USE_PSAdomain (that is, code that calls PSA crypto APIs whenUSE_PSAis enabled, and legacy crypto APIs otherwise): that’s PK, X.509, most of TLS 1.2 and the parts of TLS 1.3 that are common with TLS 1.2 or are about public/private keys (seedocs/use-psa-crypto.mdfor details).The legacy crypto domain: a number of modules there will use crypto from other modules, for example RSA and entropy will use hashes, PEM will use hashes and ciphers (from encrypted PEM), etc.
The first two categories (PSA domain, pure TLS 1.3 domain) are simple: as a
general rule, use PSA_WANT macros. (With very few exceptions, see
component_check_test_dependencies in all.sh.) In the rare instances where it is necessary to
check whether a mechanism is built-in or provided by a driver,
MBEDTLS_PSA_BUILTIN_xxx and MBEDTLS_PSA_ACCEL_xxx macros should be used
(but not legacy MBEDTLS_xxx macros).
For the USE_PSA domain, it should always be correct to use expressions like
(!USE_PSA && MBEDTLS_xxx) || (USE_PSA && PSA_WANT_xxx). Sometimes, macros
are defined in order to avoid using long expressions everywhere; they will be
mentioned in the following sections.
The remaining category, the legacy domain, tends to be more complex. There are different rules for different families of mechanisms, as detailed in the following sections.
Symmetric crypto#
Hashes#
Hash vs HMAC: Historically (since 2.0) we’ve had the generic hash
interface, and the implementation of HMAC, in the same file controlled by a
single feature macro: MBEDTLS_MD_C. This has now been split in two:
MBEDTLS_MD_LIGHTis about the generic hash interface; we could think of it asMBEDTLS_HASH_C.MBEDTLS_MD_Cis about the HMAC implementation; we could think of it asMBEDTLS_HMAC_C(auto-enablingMBEDTLS_HASH_C).
(In fact, this is not the whole story: MD_LIGHT is the core of the generic
hash interface, excluding functions such as mbedtls_md_list() and
mbedtls_md_info_from_string(), mbedtls_md_file(), etc. But I think the
above should still provide a good intuition as first approximation.)
Note that all users of hashes in the library use either the PSA Crypto API or the md.h API.
That is, no user in the library, even in the legacy domain, uses the low-level hash APIs
(mbedtls_sha256 etc). (That’s not true of all example programs, though.)
Helper macros: in config_adjust_legacy_crypto.h we define a family of
macro MBEDTLS_MD_CAN_xxx. These macros are defined (for available hashes) as
soon as MBEDTLS_MD_LIGHT is enabled. This subset of MD is automatically
enabled as soon as something from the legacy domain, or from the USE_PSA
domain, needs a hash. (Note that this includes ENTROPY_C, so in practice
MD_LIGHT is enabled in most builds.)
Note that there is a rule, enforced by config_adjust_psa_superset_legacy.h,
that as soon as PSA_CRYPTO_C is enabled, all hashes that are enabled on the
legacy side are also enabled on the PSA side (the converse is not true: a hash
that’s provided by a driver will typically be available only on the PSA side). So, in
practice, when PSA_CRYPTO_C and MD_LIGHT are both enabled,
PSA_WANT_ALG_xxx and MBEDTLS_MD_CAN_xxx are equivalent.
Legacy and USE_PSA domains: for hashes, MBEDTLS_MD_CAN_xxx (where
xxx is the legacy name of the hash) can be used everywhere (except in the
PSA domain which should use PSA_WANT as usual). No special include is
required, build_info.h or common.h is enough.
Pure TLS 1.3 domain: it is not easy to know which uses of hashes fall in
this domain as opposed to the USE_PSA domain whithout looking at the code.
Fortunately, MD_CAN and PSA_WANT macros can be used interchangeably, as
per the note above.
HMAC#
Legacy domain: the code is using the md.h API. For this domain,
availability of HMAC-xxx is determined by MBEDTLS_MD_C && MBEDTLS_MD_CAN_xxx
(see previous subsection about MD_CAN). Modules in this domain that may use
HMAC are PKCS5, PKCS7, HKDF, HMAC-DRBG and ECDSA deterministic.
USE_PSA domain: code will use the md.h API when USE_PSA is disabled,
and the psa_mac API when USE_PSA is enabled. It should check for the
availability of HMAC-xxx with either:
((!MBEDTLS_USE_PSA_CRYPTO && MBEDTLS_MD_C) ||
(MBEDTLS_USE_PSA_CRYPTO && PSA_WANT_ALG_HMAC)) &&
MBEDTLS_MD_CAN_xxx
or
(!MBEDTLS_USE_PSA_CRYPTO && MBEDTLS_MD_C && MBEDTLS_xxx_C) ||
(MBEDTLS_USE_PSA_CRYPTO && PSA_WANT_ALG_HMAC && PSA_WANT_ALG_xxx)
or any equivalent condition (see note at the end of the previous section).
The only module in this case is TLS, which currently depends on
USE_PSA_CRYPTO || MD_C.
Note: while writing this, it occurs to me that TLS 1.2 does not seem to be
checking for PSA_WANT_ALG_HMAC before enabling CBC ciphersuites when
USE_PSA is enabled, which I think it should. Builds with USE_PSA enabled,
PSA_WANT_ALG_HMAC disabled and other requirements for CBC ciphersuites
enabled, are probably broken (perhaps only at runtime when a CBC ciphersuite
is negotiated).
Pure TLS 1.3 domain: HMAC is used for the Finished message via PSA Crypto
APIs. So, TLS 1.3 should depend on PSA_WANT_ALG_HMAC - doesn’t seem to be
enforced by check_config.h, or documented in mbedtls_config.h, at the
moment.
Ciphers (AEAD and unauthenticated)#
Overview of existing (internal) APIs: we currently have 5 (families of) APIs for ciphers (and associated constructs) in the library:
Low-level API for primitives:
mbedtls_aes_xxxetc. - used bycipher.cand some other modules in the legacy domain.Internal abstraction layer
block_cipherfor AES, ARIA and Camellia primitives - used only bygcm.candccm.c, only whenCIPHER_Cis not enabled (for compatibility reasons).Block cipher modes / derivatives:
mbedtls_gcm_xxxandmbedtls_ccm_xxx, used bycipher.cand the built-in PSA implementation;mbedtls_nist_kw_xxx, used bycipher.c;mbedtls_cipher_cmac_xxx, used by the built-in PSA implementation;mbedtls_ctr_drbg_xxx, used by PSA crypto’s RNG subsystem.
Cipher: used by some modules in the legacy domain, and by the built-in PSA implementation.
PSA: used by the
USE_PSAdomain whenMBEDTLS_USE_PSA_CRYPTOis enabled.
Legacy domain: most code here is using either cipher.h or low-level APIs
like aes.h, and should use legacy macros like MBEDTLS_AES_C and
MBEDTLS_CIPHER_MODE_CBC. This includes NIST-KW, CMAC, PKCS5/PKCS12 en/decryption
functions, PEM decryption, PK parsing of encrypted keys. The only exceptions
are:
GCMandCCMuse the internal abstraction layerblock_cipherand check for availability of block ciphers usingMBEDTLS_CCM_GCM_CAN_xxxmacros defined inconfig_adjut_legacy_crypto.h. As a user, to check if AES-GCM is available through thembedtls_gcmAPI, you want to check forMBEDTLS_GCM_CandMBDTLS_CCM_GCM_CAN_AES.CTR_DRBGuses the low-levelmbedtls_aes_API if it’s available, otherwise it uses the PSA API. There is no need for users ofCTR_DRBGto check if AES is available:check_config.his already taking care of that, so from a user’s perspective as soon asMBEDTLS_CTR_DRBG_Cis enabled, you can use it without worrying about AES.
USE_PSA domain: here we should use conditions like the following in
order to test for availability of ciphers and associated modes.
// is AES available?
(!defined(MBEDTLS_USE_PSA_CRYPTO) && defined(MBEDTLS_AES_C)) || \
(defined(MBEDTLS_USE_PSA_CRYPTO) && defined(PSA_WANT_KEY_TYPE_AES))
// is CBC available?
(!defined(MBEDTLS_USE_PSA_CRYPTO) && defined(MBEDTLS_CIPHER_MODE_CBC)) || \
(defined(MBEDTLS_USE_PSA_CRYPTO) && defined(PSA_WANT_ALG_CBC_NO_PADDING))
// is GCM available?
(!defined(MBEDTLS_USE_PSA_CRYPTO) && defined(MBEDTLS_GCM_C)) || \
(defined(MBEDTLS_USE_PSA_CRYPTO) && defined(PSA_WANT_ALG_GCM))
Note: TLS is the only user of ciphers in the USE_PSA domain, and it defines
MBEDTLS_SSL_HAVE_xxx macros in config_adjust_legacy_crypto.h for the
ciphers and modes it needs to know about.
Pure TLS 1.3 domain: none. All from TLS 1.3 are in the USE_PSA domain
(common to TLS 1.2).
Key derivation#
Legacy domain: the modules PKCS5 and PKCS12 both provide key derivation (respectively PBKDF2-HMAC and PKCS12 derivation), and use it for password-based encryption. (Note: PEM has an implementation of PBKDF1 but it’s internal.)
USE_PSA domain: PK (parse) will use PKCS5 and PKCS12 encryption (hence
indirectly key derivation) if present in the build. The macros are
MBEDTLS_PKCS5_C and MBEDTLS_PKCS12_C. Note that even when USE_PSA is
enabled, PK parse will not use PSA for the PBKDF2 part of PKCS5 decryption.
Pure TLS 1.3 domain: TLS 1.3 is using HKDF via PSA Crypto APIs. We already
enforce in check_config.h that TLS 1.3 depends on the appropriate PSA_WANT
macros.
Asymmetric crypto#
RSA#
Legacy domain and USE_PSA domain: use RSA_C everywhere. (Note: there’s
no user of RSA in the legacy domain, and the only direct user in the USE_PSA
domain is PK - both X.509 and TLS will only RSA via PK.)
Pure TLS 1.3 domain: no use of RSA in this domain. All TLS 1.3 uses of RSA
go through PK, hence are in the USE_PSA domain.
FFDH#
Legacy domain and USE_PSA domain: use DHM_C. The only user is TLS 1.2
which is actually in the legacy domain - this is an exception where USE_PSA
has no effect, because PSA doesn’t cover the needs of TLS 1.2 here.
Pure TLS 1.3 domain: use PSA_WANT. The TLS 1.3 code for Diffie-Hellman
is common to ECDH and FFDH thanks to PSA Crypto APIs being generic enough. The
parts about FFDH are guarded with PSA_WANT_ALG_FFDH (with the reasoning that
this implies support for the corresponding key type).
ECC#
Curves: in config_adjut_psa_superset_legacy.h we ensure that, as soon as
PSA_CRYPTO_C is enabled, all
curves that are supported on the legacy side (MBEDTLS_ECP_DP_xxx_ENABLED)
are also supported on the PSA side (PSA_WANT_ECC_xxx). (The converse is not
true as a curve provided by a driver will typically only be available on the
PSA side).
In config_adjust_legacy_crypto.h we define macros MBEDTLS_ECP_HAVE_xxx.
These macros are useful for data and functions that have users in several
domains, such as mbedtls_ecc_group_to_psa(), or that have users only in the
USE_PSA domain but want a simpler (if sub-optimal) condition, such as
mbedtls_oid_get_ec_grp().
Strictly speaking, code in the USE_PSA domain should not use the above
MBEDTLS_ECP_HAVE_xxx macros but conditions like
(!MBEDTLS_USE_PSA_CRYPTO && MBEDTLS_ECP_DP_xxx_ENABLED) ||
(MBEDTLS_USE_PSA_CRYPTO && PSA_WANT_ECC_xxx)
Note while writing: a lot of tests for things in the USE_PSA domain appear
to be using MBEDTLS_ECP_HAVE_xxx. IMO this is incorrect, but not caught by
the CI because I guess we don’t run tests in configurations that have both
USE_PSA_CRYPTO disabled, and some curves enabled only on the PSA side. My
initial feeling is we don’t care about such configurations as this point, and
can leave the dependencies as they are until they’re replaced with PSA_WANT
macros in 4.0 anyway.
Legacy domain: use the legacy macros ECP_C, ECDH_C, ECDSA_C,
ECJPAKE_C, MBEDTLS_ECP_DP_xxx_ENABLED. (This is mostly just ECDH, ECDSA
and EC J-PAKE using ECP.)
Key management, USE_PSA domain: MBEDTLS_PK_HAVE_ECC_KEYS means that PK
supports ECC key parsing and writing (and storage). It does not imply support
for doing crypto operation with such keys - see MBEDTLS_PK_CAN_ECDSA_xxx
above for that.
ECDH, USE_PSA domain: this is just TLS 1.2. It’s using the helper macro
MBEDTLS_CAN_ECDH defined in config_adjust_legacy_crypto.h (which should
probably be called MBEDTLS_SSL_TLS1_2_CAN_ECDH as it’s only for TLS 1.2).
(Note: the macro is not used directly in the code, it’s only used as a
dependency for relevant TLS 1.2 key exchanges. Then the code uses the guards
for the key exchanges.)
ECDH, pure TLS 1.3 domain: using PSA_WANT_ALG_ECDH.
ECDSA, USE_PSA domain: should use the macros
MBEDTLS_PK_CAN_ECDSA_{SIGN,VERIFY,SOME} that indicate support for signature
generation, verification, or at least one of those, respectively. To check for
support for signatures with a specific hash, combine
MBEDTLS_PK_CAN_ECDSA_xxx with MBEDTLS_MD_CAN_xxx.
ECDSA, pure TLS 1.3 domain: none - everything goes through PK.
EC J-PAKE, USE_PSA domain: only used by TLS 1.2. The code is guarded by
the corresponding KEY_EXCHANGE macro, which in check_config.h depends on
the appropriate macros depending on whether USE_PSA is on or off.
EC J-PAKE, pure TLS 1.3 domain: none - EC J-PAKE is TLS 1.2 (so far).
Related internal macros:
MBEDTLS_PK_USE_PSA_EC_DATAis an internal switch of the PK module. When it’s not defined, PK stores ECC keys as astruct mbedtls_ecxxx_keypair; when it’s defined, PK stores in a PSA -friendly format instead (PSA key slot for private keys, metadata + array of bytes with the PSA import/export format for the public part). This macro is only defined whenECP_Cis not andUSE_PSAis, see comments above its definition inpk.hfor details.MBEDTLS_ECP_LIGHTenables only a subset ofecp.c. This subset is pretty much ad hoc: it’s basically everything that doesn’t depend on scalar multiplication (the complex expensive operation in ECC arithmetic). Basically, this subset gives access to curve data (constants), key storage, basic parsing and writing. It is auto-enabled in some driver-only configurations where the user has disabledECP_Cbecause they have drivers for the crypto operations they use, but they’ve also asked for some things that are not supported by drivers yet, such as deterministic key derivation, or parsing of compressed keys - on those cases,ECP_LIGHTwill support this needs without bringing back the fullECP_C.