This document describes the compile-time configuration option
MBEDTLS_USE_PSA_CRYPTO from a user’s perspective.
This option:
makes the X.509 and TLS libraries use PSA for cryptographic operations as much as possible, see “Internal changes” below;
enables new APIs for using keys handled by PSA Crypto, such as
mbedtls_pk_setup_opaque()andmbedtls_ssl_conf_psk_opaque(), see “New APIs / API extensions” below.
General considerations#
Application code: when this option is enabled, you need to call
psa_crypto_init() before calling any function from the SSL/TLS, X.509 or PK
modules, except for the various mbedtls_xxx_init() functions which can be called
at any time.
Why enable this option: to fully take advantage of PSA drivers in PK, X.509 and TLS. For example, enabling this option is what allows use of drivers for ECDSA, ECDH and EC J-PAKE in those modules. However, note that even with this option disabled, some code in PK, X.509, TLS or the crypto library might still use PSA drivers, if it can determine it’s safe to do so; currently that’s the case for hashes.
Relationship with other options: This option depends on
MBEDTLS_PSA_CRYPTO_C. These two options differ in the following way:
MBEDTLS_PSA_CRYPTO_Cenables the implementation of the PSA Crypto API. When it is enabled,psa_xxx()APIs are available and you must callpsa_crypto_init()before you call any otherpsa_xxx()function. Other modules in the library (non-PSA crypto APIs, X.509, TLS) may or may not use PSA Crypto but you’re not required to callpsa_crypto_init()before calling non-PSA functions, unless explicitly documented (TLS 1.3).MBEDTLS_USE_PSA_CRYPTOmeans that X.509 and TLS will use PSA Crypto as much as possible (that is, everywhere except for features that are not supported by PSA Crypto, see “Internal Changes” below for a complete list of exceptions). When it is enabled, you need to callpsa_crypto_init()before calling any function from PK, X.509 or TLS; however it doesn’t change anything for the rest of the library.
Scope: MBEDTLS_USE_PSA_CRYPTO has no effect on modules other than PK,
X.509 and TLS. It also has no effect on most of the TLS 1.3 code, which always
uses PSA crypto. The parts of the TLS 1.3 code that will use PSA Crypto or not
depending on this option being set or not are:
record protection;
running handshake hash;
asymmetric signature verification & generation;
X.509 certificate chain verification. You need to enable
MBEDTLS_USE_PSA_CRYPTOif you want TLS 1.3 to use PSA everywhere.
Historical note: This option was introduced at a time when PSA Crypto was
still beta and not ready for production, so we made its use in X.509 and TLS
opt-in: by default, these modules would keep using the stable,
production-ready legacy (pre-PSA) crypto APIs. So, the scope of was X.509 and
TLS, as well as some of PK for technical reasons. Nowadays PSA Crypto is no
longer beta, and production quality, so there’s no longer any reason to make
its use in other modules opt-in. However, PSA Crypto functions require that
psa_crypto_init() has been called before their use, and for backwards
compatibility reasons we can’t impose this requirement on non-PSA functions
that didn’t have such a requirement before. So, nowadays the main meaning of
MBEDTLS_USE_PSA_CRYPTO is that the user promises to call psa_crypto_init()
before calling any PK, X.509 or TLS functions. For the same compatibility
reasons, we can’t extend its scope. However, new modules in the library, such
as TLS 1.3, can be introduced with a requirement to call psa_crypto_init().
New APIs / API extensions#
PSA-held (opaque) keys in the PK layer#
New API function: mbedtls_pk_setup_opaque() - can be used to
wrap a PSA key pair into a PK context. The key can be used for private-key
operations and its public part can be exported.
Benefits: isolation of long-term secrets, use of PSA Crypto drivers.
Limitations: please refer to the documentation of mbedtls_pk_setup_opaque()
for a full list of supported operations and limitations.
Use in X.509 and TLS: opt-in. The application needs to construct the PK context using the new API in order to get the benefits; it can then pass the resulting context to the following existing APIs:
mbedtls_ssl_conf_own_cert()ormbedtls_ssl_set_hs_own_cert()to use the key together with a certificate for certificate-based key exchanges;mbedtls_x509write_csr_set_key()to generate a CSR (certificate signature request);mbedtls_x509write_crt_set_issuer_key()to generate a certificate.
PSA-held (opaque) keys for TLS 1.2 EC J-PAKE key exchange#
New API function: mbedtls_ssl_set_hs_ecjpake_password_opaque().
Call this function from an application to register a PSA key for use with the
TLS 1.2 EC J-PAKE key exchange.
Benefits: isolation of long-term secrets.
Limitations: none.
Use in TLS: opt-in. The application needs to register the key using one of the new APIs to get the benefits.
PSA-based operations in the Cipher layer#
There is a new API function mbedtls_cipher_setup_psa() to set up a context
that will call PSA to store the key and perform the operations.
This function only worked for a small number of ciphers. It is now deprecated
and it is recommended to use psa_cipher_xxx() or psa_aead_xxx() functions
directly instead.
Warning: This function will be removed in a future version of Mbed TLS. If you are using it and would like us to keep it, please let us know about your use case.
Internal changes#
All of these internal changes are active as soon as MBEDTLS_USE_PSA_CRYPTO
is enabled, no change required on the application side.
TLS: most crypto operations based on PSA#
Current exceptions:
Finite-field (non-EC) Diffie-Hellman (used in key exchanges: DHE-RSA, DHE-PSK).
Restartable operations when
MBEDTLS_ECP_RESTARTABLEis also enabled (see the documentation of that option).
Other than the above exceptions, all crypto operations are based on PSA when
MBEDTLS_USE_PSA_CRYPTO is enabled.
X.509: most crypto operations based on PSA#
Current exceptions:
Restartable operations when
MBEDTLS_ECP_RESTARTABLEis also enabled (see the documentation of that option).
Other than the above exception, all crypto operations are based on PSA when
MBEDTLS_USE_PSA_CRYPTO is enabled.
PK layer: most crypto operations based on PSA#
Current exceptions:
Verification of RSA-PSS signatures with an MGF hash that’s different from the message hash.
Restartable operations when
MBEDTLS_ECP_RESTARTABLEis also enabled (see the documentation of that option).
Other than the above exceptions, all crypto operations are based on PSA when
MBEDTLS_USE_PSA_CRYPTO is enabled.