Overview

These are the release notes for the LPC540xx/LPC54S0xx Flashloader. For additional information and getting started instructions, check Getting Started section of this document.

The device Flashloader is an application that is loaded into the internal RAM of the device. The Flashloader is designed to work as a second stage bootloader for this device. It detects communication on one of the supported peripherals (USB-HID or UART), downloads a user application, and writes the application to external serial NOR device. The Flashloader is initially loaded by MfgTool which then helps in programming the flash.

This release includes the PC-hosted blhost application. This blhost is used for downloading user-application to flash device in both development and production phase while device is running flashloader application and connected to PC Host.