Features
For downloading an application, the Flashloader supports the following communication interfaces:
USB-HID
LPUART1
It also supports configuring and programming the external flash device in a user-friendly manner. For further details, refer to MCU Flashloader Reference Manual.