The Header File Config System#
The header file configurations system is used to fine-tune component options.
The following diagram shows how the system works.
Source files shall include config_tfm.h when necessary to fetch Component option settings.
It is expected that all Component options are included in config_tfm.h to explicitly set values
for each option.
The config_tfm.h includes base configuration config_base.h. Refer to
Base_configuration for details of the base configurations.
The config_tfm.h includes a customized project config file provided via compile definition
PROJECT_CONFIG_HEADER_FILE. Customized Component options in the project config file overrides
those configured in config_base.h.
The project config header file can be
Generated by the TF-M Kconfig system <kconfig_system>
One of the header files of Profiles <tf-m_profiles>, set via the
TFM_PROFILEbuild option.Manually customized profile based on pre-set profiles.
Users set CMake variable PROJECT_CONFIG_HEADER_FILE with the full path of the configuration
header file.
A platform can adjust or place restriction on config options by providing a config_tfm_target.h
under the root folder of their platforms.
If the build system finds the file, it sets the TARGET_CONFIG_HEADER_FILE compile definition.
Platform specific option settings in TARGET_CONFIG_HEADER_FILE overrides those configured in
config_base.h.
#ifdef TARGET_CONFIG_HEADER_FILE
#include TARGET_CONFIG_HEADER_FILE
#endif
#ifdef PROJECT_CONFIG_HEADER_FILE
#include PROJECT_CONFIG_HEADER_FILE
#endif
#include "config_base.h"
Each component can implement a config_<comp_name>_check.h to validate component specific config
dependencies. config_<comp_name>_check.h shall include config_tfm.h
Copyright (c) 2022, Arm Limited. All rights reserved.