Firmware Update Service#
- Author:
Sherry Zhang
- Organization:
Arm Limited
- Contact:
Sherry Zhang <Sherry.Zhang2@arm.com>
Introduction of Firmware Update service#
The Firmware Update(FWU) service provides the functionality of updating firmware images. It provides a standard interface for updating firmware and it is platform independent. TF-M defines a shim layer to support cooperation between bootloader and FWU service.
This partition supports the following features:
Query the firmware store information.
Image preparation: prepare a new firmware image in the component’s firmware store.
Image installation: install prepared firmware images on all components that have been prepared for installation.
Image trial: manage a trial of new firmware images atomically on all components that are in TRIAL state.
A typical flow through the component states is shown below 1PSA Firwmare Update API.
Components#
- The structure of the TF-M Firmware Update service is listed below:
Component name
Description
Location
Client API interface
This module exports the client API of PSA Firmware Update to the users.
./interface/src/tfm_fwu_api.cManifest
The manifest file is a description of the service components.
./secure_fw/partitions/firmware_update/tfm_firmware_update.yamlNSPE client API interface
This module exports the client API of PSA Firmware Update to the NSPE(i.e. to the applications).
./interface/src/tfm_fwu_api.cIPC request handlers
This module handles all the secure requests in IPC model. It maitains the image state context and calls the image ID converter to achieve the firmware update functionalities.
./secure_fw/partitions/firmware_update/tfm_fwu_req_mngr.cShim layer between FWU and bootloader
This module provides the APIs with the functionality of operating the bootloader to cooperate with the Firmware Update service
./secure_fw/partitions/firmware_update/bootloader/tfm_bootloader_fwu_abstraction.hShim layer example based on MCUboot
This module is the implementation of the shim layer between FWU and bootloader based on MCUboot.
./secure_fw/partitions/firmware_update/bootloader/mcuboot/tfm_mcuboot_fwu.c
Service API description#
This service follows the PSA Firmware Update API spec of version 1.0 [1]. Please refer to Firmware Update spec for the detailed description.
Shim Layer between FWU and bootloader#
The firmware update operations are achieved by calling the shim layer APIs between bootloader and FWU.
Shim layer introduction#
This shim layer provides the APIs with the functionality of operating the
bootloader to cooperate with the Firmware Update service. This shim layer
is decoupled from bootloader implementation. Users can specify a specific
bootloader by setting TFM_FWU_BOOTLOADER_LIB build configuration and
adding the specific build scripts into that file. By default, the MCUboot
is chosen as the bootloader.
Interfaces of the shim Layer#
fwu_bootloader_init(function)#
Prototype#
psa_status_t fwu_bootloader_init(void);
Description#
Bootloader related initialization for the firmware update. It reads some necessary shared data from the memory if needed. It initializes the flash drivers defined in FLASH_DRIVER_LIST. Platform can define FLASH_DRIVER_LIST in flash_layout.h to overload the default driver list.
Parameters#
N/A
fwu_bootloader_staging_area_init(function)#
Prototype
psa_status_t fwu_bootloader_staging_area_init(psa_fwu_component_t component,
const void *manifest,
size_t manifest_size);
Description
The component is in READY state. Prepare the staging area of the component for image download. For example, initialize the staging area, open the flash area, and so on.
Parameters
component: The identifier of the target component in bootloader.manifest: A pointer to a buffer containing a detached manifest for the update. If the manifest is bundled with the firmware image, manifest must be NULL.manifest_size: Size of the manifest buffer in bytes.
fwu_bootloader_load_image(function)#
Prototype
psa_status_t fwu_bootloader_load_image(psa_fwu_component_t component,
size_t image_offset,
const void *block,
size_t block_size);
Description
Load the image into the target component.
Parameters
component: The identifier of the target component in bootloader.image_offset: The offset of the image being passed into block, in bytes.block: A buffer containing a block of image data. This might be a complete image or a subset.block_size: Size of block.
fwu_bootloader_install_image(function)#
Prototype
psa_status_t fwu_bootloader_install_image(psa_fwu_component_t *candidates,
uint8_t number);
Description
Check the authenticity and integrity of the image. If a reboot is required to complete the check, then mark this image as a candidate so that the next time bootloader runs it will take this image as a candidate one to bootup. Return the error code PSA_SUCCESS_REBOOT.
Parameters
candidates: A list of components in CANDIDATE state.number: Number of components in CANDIDATE state.
fwu_bootloader_mark_image_accepted(function)#
Prototype
psa_status_t fwu_bootloader_mark_image_accepted(const psa_fwu_component_t *trials,
uint8_t number);
Description
Call this API to mark the TRIAL(running) image in component as confirmed to avoid revert when next time bootup. Usually, this API is called after the running images have been verified as valid.
Parameters
trials: A list of components in TRIAL state.number: Number of components in TRIAL state.
fwu_bootloader_reject_staged_image(function)#
Prototype
psa_status_t fwu_bootloader_reject_staged_image(psa_fwu_component_t component);
Description
The component is in STAGED state. Call this API to Uninstall the staged image in the component so that this image will not be treated as a candidate next time bootup.
Parameters
component: The identifier of the target component in bootloader.
fwu_bootloader_reject_trial_image(function)#
Prototype
psa_status_t fwu_bootloader_reject_trial_image(psa_fwu_component_t component);
Description
The component is in TRIAL state. Mark the running image in the component as rejected.
Parameters
component: The identifier of the target component in bootloader.
fwu_bootloader_clean_component(function)#
Prototype
psa_status_t fwu_bootloader_clean_component(psa_fwu_component_t component);
Description
The component is in FAILED or UPDATED state. Clean the staging area of the component.
Parameters
component: The identifier of the target component in bootloader.
fwu_bootloader_get_image_info(function)#
Prototype
psa_status_t fwu_bootloader_get_image_info(psa_fwu_component_t component,
bool query_state,
bool query_impl_info,
psa_fwu_component_info_t *info);
Description
Get the image information of the given bootloader_image_id in the staging area or the running area.
Parameters
component: The identifier of the target component in bootloader.
query_state: Whether query the ‘state’ field of psa_fwu_component_info_t.
query_impl_info: Whether Query ‘impl’ field of psa_fwu_component_info_t.
info: Buffer containing return the component information.
Limitations of current implementation#
Currently, the MCUboot based implementation does not record image update results like failure or
success. And FWU partition does not detect failure errors in bootloader installation. If an image
installation fails in the bootloader and the old image still runs after reboot, PSA_FWU_READY
state will be returned by psa_fwu_query() after reboot.
Currently, image download recovery after a reboot is not supported. If a reboot happens in image preparation, the downloaded image data will be ignored after the reboot.
Benefits Analysis on this Partition#
Implement the FWU functionality in the non-secure side#
The APIs listed in PSA Firmware Update API spec [1] can also be implemented in the non-secure side.
Pros and Cons for implementing FWU APIs in secure side#
Pros#
It protects the image in the passive or staging area from being tampered with by the NSPE. Otherwise, a malicious actor from NSPE can tamper the image stored in the non-secure area to break image update.
It protects secure image information from disclosure. In some cases, the non-secure side shall not be permitted to get secure image information.
It protects the active image from being manipulated by NSPE. Some bootloader supports testing the image. After the image is successfully installed and starts to run, the user should set the image as permanent image if the image passes the test. To achieve this, the area of the active image needs to be accessed. In this case, implementing FWU service in SPE can prevent NSPE from manipulating the active image area.
On some devices, such as the Arm Musca-B1 board, the passive or staging area is restricted as secure access only. In this case, the FWU partition should be implemented in the secure side.
Cons#
It increases the image size of the secure image.
It increases the execution latency and footprint. Compared to implementing FWU in NSPE directly, calling the Firmware Update APIs which are implemented in the secure side increases the execution latency and footprint.
It can increase the attack surface of the secure runtime.
Users can decide whether to call the FWU service in TF-M directly or implement the Firmware Update APIs in the non-secure side based on the pros and cons analysis above.
Reference#
Copyright (c) 2021-2022, Arm Limited. All rights reserved.