MCUXpresso SDK Documentation

Platform Documentation

Platform Documentation#

This document describes conventions for platform documentation for easy and smooth integration into TF-M online documentation.

Principles#

  • Minimise TF-M requirements and maximise flexibility to let platform vendors reuse existing documentation.

  • Platforms are grouped under vendors’ name. There is space to keep general information not specific to any of the vendors’ platforms.

  • A Table Of Contents (TOC) structures platforms’ documentation. There is no defined template for platform documents.

Rules#

  • Platforms documentation is gathered in /docs/platform folder. This folder is similar to the platforms implementation folder /platform/ext/target but does not need to mirror its structure.

  • A vendor is represented by a subfolder with index.rst as an entry point. This file may contain general materials about a vendor not specific to a particular platform.

  • A vendor’s index.rst shall carry a TOCtree structure with a list of all supported platforms at the top level.

  • An explicit platform name is preferred in a vendor’s TOCtree instead of use of platform’s title by default.

Note

Do not forget to update the summary file after adding a new platform /docs/platform/platform_introduction.rst included into TF-M introduction.

Example#

Assuming a vendor ABCD123 wants to add and document a new platform Secure 1024 in TF-M. Here are the basic steps:

  1. Create a folder /docs/platform/ABCD123/

  2. Create a platform documentation under /docs/platform/ABCD123. A natural choice is to put a new platform under /docs/platform/ABCD123/Secure_1024 folder but it’s not required.

  3. Create a file /docs/platform/ABCD123/index.rst with a platform entry, presuming it’s location in /docs/platform/ABCD123/Secure_1024/index.rst:

#################
ABCD123 platforms
#################

.. toctree::
Secure 1024 <Secure_1024/index>
  1. Finally, update /docs/platform/index.rst with a new vendor name:

##############
TF-M Platforms
##############

.. toctree::
    :maxdepth: 2
    :glob:

    Arm <arm/index.rst>
    NXP <nxp/index.rst>
    Cypress <cypress/index.rst>
    ...
    ABCD123 <ABCD123/index.rst>

Copyright (c) 2023, Arm Limited. All rights reserved.