MCUXpresso SDK Documentation

Source Structure#

TF-M is designed to provide a user-friendly source structure to ease integration and service development. This document introduces the source structure and its design intention of TF-M. Additionally, the folders below are important for TF-M integration and descibed in a separate documents:

/ (TF-M root)#

This table describes the structure under the root folder with part of possible folders.

Folder name

Description

bl1

The 1st stage immutable bootloader

bl2

MCUBoot based 2nd stage bootloader

cmake

Cmake files of the build system

config

Configuration system files

docs

The documentation

interface

RoT service API for client calls

lib

The 3rd party libraries

platform

Platform intermedia files

secure_fw

The secure firmware

tools

Tools in scripts for building

platform#

The platform folder contains SW ports of all supported platforms and the files necessary for adding a new platform. Please refer to platform folder document for more information.

Folder name

Description

include

HAL and platform public headers

ext

Platform ports and related files

platform/ext#

This folder can include imported files licensed differently from TF-M’s BSD-3 license. More details are in the dedicated document Details for the platform/ext folder.

Folder name

Description

accelerator

Supported Crypto HW accelerators

cmsis

A copy of essential CMSIS headers

common

Common HAL implementation

driver

Driver headers for porting

target/<vendor>

Vendor specific folders with ported platforms

Each vendor is assigned one folder for usage under target/. A vendor contributes platform’s ports and manages the structure inside it.

secure_fw#

This folder contains components needed by secure firmware and the exported interfaces for application, service development and HAL integration.

Folder name

Description

include

Public headers of secure_fw

partitions

Default services and SPRTL

spm

PSA FF-M SPM implementation

shared

Sources shared out of SPRTL

The shared sources can be referenced by the building system out of SPRTL. Generally, they are runtime and PSA APIs.

secure_fw/include#

This folder holds public headers for external references by clients, services and platforms. Avoid putting private headers, not referenced by other modules in this include folder.

secure_fw/partitions#

This folder contains default services implemented as partitions and runtime utilities used and provided by TF-M.

Folder name

Description

lib/runtime

The SPRTL sources and intermedia files

<partition_x>

Sources of partition_x

<partition_x>/include

RoT Service API headers of partition_x

<partition_y>

Sources of partition_y

<partition_y>/include

RoT Service API headers of partition_y

Here partition_x and partition_y are examples of RoT services without detailed structure of them.

secure_fw/spm#

The SPM is the core component to provide a mechanism for providing secure services complied with PSA FF-M.

Folder name

Description

include

SPM public headers.

core

SPM base functionalities

*ext

Extended SPM functionalities


Copyright (c) 2020-2023, Arm Limited. All rights reserved.