Advisory TFMV-7#
Title |
ARoT can access PRoT data via debug logging functionality |
|---|---|
CVE ID |
|
Public Disclosure Date |
The issue was publicly reported on 2023.12.04 |
Versions Affected |
All version up to TF-M v2.0.0 inclusive |
Configurations |
IPC mode with TFM_SP_LOG_RAW_ENABLED=1 |
Impact |
A malicious ARoT partition can expose any part of memory via stdio interface if TFM_SP_LOG_RAW_ENABLED is set |
Fix Version |
TBD |
Credit |
Roman Mazurak, Infineon |
Background#
TF-M log subsystem if enabled by TFM_SP_LOG_RAW_ENABLED config option,
uses a SVC call to print logging messages on the stdio output interface.
Since the SVC handler has the highest privilege level and full memory
access, this communication channel can be exploited to expose any memory content
to stdout device, usually UART.
The logging subsystem is available to the secure side only but in isolation
level 2 and higher PSA Root of Trust partitions (PRoT) shall be protected
from an access from Application Root of Trust (ARoT) partitions. Although
a direct call of tfm_hal_output_sp_log() from ARoT partition will be
blocked by MPU raising the MemoryManagement() exception, a malicious
ARoT partition can create an alternative SVC call to output any memory
data like this:
static int tfm_output_unpriv_string(const unsigned char *str, size_t len)
{
__ASM volatile("SVC %0 \n"
"BX LR \n"
: : "I" (2));
}
Impact#
In IPC mode with PSA isolation level 2 and higher and TFM_SP_LOG_RAW_ENABLED
option enabled an ARoT partition can expose to the stdout device any memory
data using TF-M logging subsystem via SVC call.
Mitigation#
Ensure that data sent for logging belongs to the current partition. For that purpose
tfm_hal_memory_check(curr_partition->boundary, data, size, TFM_HAL_ACCESS_READABLE)
is added to the logging function of the SVC handler. If the check fails
then tfm_core_panic() is invoked and system halts.
Copyright (c) 2024, Arm Limited. All rights reserved.