MCUXpresso SDK Documentation

Advisory TFMV-5

Advisory TFMV-5#

Title

psa_fwu_write() may cause buffer overflow in SPE.

CVE ID

CVE-2021-43619

Public Disclosure Date

Feb 11, 2022

Versions Affected

From 3e7129f to 921d0ea

Configurations

IPC model with Firmware Update partition enabled

Impact

In IPC model, the caller of psa_fwu_write() from SPE or NSPE can overwrite the stack memory outside of the local buffer in Firmware Update partition.

Fix Version

commit 78f7530

Credit

Mark Horvath, Staff Software Engineer from Arm Ltd.

Background#

In Firmware Update partition, the psa_fwu_write() service is declared as:

/**
 * \brief Writes an image to its staging area.
 *
 * Writes the image data 'block' with length 'block_size' to its staging area.
 *
 * \param[in] image_id        The identifier of the image
 * \param[in] block_offset    The offset of the block being passed into block,
 *                            in bytes
 * \param[in] block           A buffer containing a block of image data. This
 *                            might be a complete image or a subset.
 * \param[in] block_size      Size of block. The size must not be greater than
 *                            PSA_FWU_MAX_BLOCK_SIZE.
 *
 */
psa_status_t psa_fwu_write(psa_image_id_t image_id,
                           size_t block_offset,
                           const void *block,
                           size_t block_size);

In IPC model, this service calls the tfm_fwu_write_ipc() API to write the input data into the device. In this API, the block_size bytes input data (in block argument) is read into a 1024 bytes local buffer via the psa_read() API. If the input argument block_size is greater than 1024, then the memory space starting from the address of the local buffer with block_size bytes would be overwritten by the input data in block argument.

Impact#

In IPC model, the caller of psa_fwu_write() from SPE or NSPE can overwrite the memory space in RAM. The overwritten memory space ranges from the address of the local buffer which locates at the stack of Firmware Update partition to the end of the RAM. The overwritten memory may include the data of SPM and device drivers, as well as part of the stack of Firmware Update partition.

Mitigation#

Add check against the input buffer length in the tfm_fwu_write_ipc() API before reading the input data into the local buffer. See commit 78f7530.


Copyright (c) 2022, Arm Limited. All rights reserved.