MCUXpresso SDK Documentation

Intrusion Detection System#

The Intrusion Detection System (IDS) is a proprietary feature which allows the Car Anchor to monitor anomalous events related to the traffic and conditions generated during the operation of the Bluetooth LE software stack. These events are detected at Host and Controller level. The application registers a callback where it receives and handles reports.

The IDS feature is supported on the following platforms:

  • KW45B41Z-EVK

  • KW47-EVK

To enable IDS, modify the Digital Key Car Anchor as per the steps listed below:

  • In app_preinclude.h file, set gIntrusionDetectionSystem_d to 1.

Intrusion Detection System Test Mode#

The IDS Test Mode is a development and testing feature that allows developers to simulate and validate IDS security event detection without requiring actual attack scenarios or malicious devices.

Enabling Test Mode#

To enable IDS Test Mode, set gIntrusionDetectionSystemTestMode_d to 1 in app_preinclude.h.

This enables:

  • Shell command idstest for triggering security events

  • Pairing message interception hooks

  • Test packet generation utilities

Supported Security Events#

IDS Test Mode supports triggering the following security events:

Bit

Event Macro

Description

Category

Trigger Method

0

gSecEvt_Sweyntooth_MaxEncKeySize_c

Max Encryption Key Size (Sweyntooth)

Pairing

Hook

1

gSecEvt_DhKeyCheckZero_c

DH Key Check Zero

Pairing

Hook

2

gSecEvt_UnexpectedSmpMessage_c

Unexpected SMP Message

Pairing

Hook

5

gSecEvt_MicFailureDisconnect_c

MIC Failure Disconnect

Connection

Packet

6

gSecEvt_EncReqNonBonded_c

Non-Bonded Device

Connection

Packet

7

gSecEvt_MalformedL2cap_c

Malformed L2CAP Packet

Connection

Packet

8

gSecEvt_MalformedAtt_c

Malformed ATT Packet

Connection

Packet

13

gSecEvt_ForcedRepairing_c

Forced Re-pairing

Pairing

Hook

14

gSecEvt_L2capFragmentsExceedMTU_c

L2CAP Fragments Exceed MTU (Blue Frag)

Connection

Packet

16

gSecEvt_KNOB_c

Key Negotiation over Bluetooth (KNOB)

Pairing

Hook

18

gSecEvt_InvalidPublicKey_c

Invalid Public Key

Pairing

Hook

19

gSecEvt_WrongConfirmValue_c

Wrong Confirm Value

Pairing

Hook

20

gSecEvt_DHKeyCheckFailed_c

DH Key Check Failed

Pairing

Hook

Event Categories#

Connection Events (Immediate Trigger)#

These events are triggered immediately when the idstest command is executed:

  • BIT5: MIC Failure Disconnect

  • BIT7: Malformed L2CAP Packet

  • BIT8: Malformed ATT Packet

  • BIT14: L2CAP Fragments Exceed MTU

BIT6: Encryption Request from Non-Bonded Device#

Natural Scenario:

  1. Connect device to anchor with bonding enabled

  2. Complete pairing and bonding successfully

  3. Disconnect device

  4. On anchor: Run factoryreset command

  5. On device: Reconnect without clearing bonds

  6. IDS event triggers when device sends encryption request

Pairing Events (Hook-based Trigger)#

These events activate a message interception hook and trigger during the next pairing procedure:

  • BIT0: Sweyntooth Max Encryption Key Size

  • BIT1: DH Key Check Zero

  • BIT2: Unexpected SMP Message

  • BIT13: Forced Re-pairing

  • BIT16: KNOB (Key Negotiation)

  • BIT18: Invalid Public Key

  • BIT19: Wrong Confirm Value

  • BIT20: DH Key Check Failed

Using the idstest Command#

idstest <event_bit> [device_id]

Examples#

Trigger Connection Event (Immediate):

Anchor> idstest 5 0
[IDS TEST] Event BIT5 (mask 0x20000000) triggered for device 0.
Anchor> Received IDS event 32 triggered by peer 25008F195173

Trigger Pairing Event (During Next Pairing):

Anchor> idstest 0 0
[IDS TEST] Pairing event BIT0 (mask 0x00000001) will be triggered on next pairing.
[IDS TEST] Hook activated. Now run 'sd op' to start Owner Pairing.

Anchor> sd op
Advertising started - Legacy.
Connected!
Received IDS event 65536 triggered by peer 1BE0914D955A