MCUXpresso SDK Documentation

Prerequisites

Prerequisites#

The Bluetooth Low Energy Connection Handover feature can be integrated in an application that fulfills the following requirements:

  • Supported platforms: KW45, KW47 and KW43.

  • Bluetooth Low Energy application that is using the lib_ble_OPT_host_cm33_iar.a host library.

  • Communication channel between the Source and Target devices involved in the Connection Handover procedure.