MCUXpresso SDK Documentation

Case 1 (Bluetooth LE)

Case 1 (Bluetooth LE)#

  1. Open a serial port terminal and connect to the two boards, in the same manner described in Testing devices. The figure below displays the start screen after the board is reset.

    Tera Term – Hybrid Wireless UART (Bluetooth LE) - Generic FSK start screen Tera Term – Hybrid Wireless UART (Bluetooth LE) - Generic FSK start screen

  2. The application starts as a GAP central. To switch the role to a GAP peripheral, press the ROLESW button. Depending on the role, when pressing the SCANSW button, the application starts either scanning or advertising.

  3. As soon as the CONNLED turns solid on both devices, the user can start writing in one of the consoles. The text appears on the other terminal.

  4. After creating a connection, the role (central or peripheral) is displayed on the console. The role switch can be pressed again before creating a new connection. An output example can be observed in the figure below.

    Tera Term – received text on Wireless UART (Bluetooth LE) Tera Term – received text on Wireless UART (Bluetooth LE)

Parent topic:Usage