MCUXpresso SDK Documentation

Case 2 (Generic FSK)

Case 2 (Generic FSK)#

When operating the Generic FSK mode, the following steps should be followed.

  1. Open a serial port terminal and connect to the two boards, in the same manner described in Testing devices. The start screen after the board is reset is the same as in Figure.

  2. The Generic FSK communication direction is not preset. To start receiving, double click the SCANSW button on one board. Then, the device starts receiving packets on the same channel as the Bluetooth LE channel 37.

  3. To start transmitting, long press the ROLESW button on the other board. The transmitting device uses an identifier known by the receiver and its packets are displayed in the CLI as shown in Figure:

    Teraterm – packet transmit/receive on Generic FSK

  4. To stop Generic FSK reception, double click the ROLESW button.

  5. To stop the periodic Generic FSK transmit operation, long press the ROLESW button again, if the transmit procedure is ongoing. The long press of the ROLESW button acts as a toggle for the transmit. At this point, both devices can reverse the direction of communication by following the exact same steps.

    See Figure.

    Tera Term – stop Generic FSK activity

Parent topic:Usage