power_mode_switch_bm_pmic_rt1xxx_core#
Overview#
The Power mode switch bm pmic demo application demonstrates the usage of chip’s power features with integration of PF5020. The CPU mode is power mode of CPU platform. Each CPU platform has its own power mode. They are RUN, WAIT, STOP, SUSPEND. Some resource that are managed at system level, and are not owned and controlled by any of the CPU platform are called as public resources. Set point is used to control the power state of the public resources. With CPU Mode and Set Point defined properly, the Power Mode of a system is defined as a combination of the CPU Mode and Set Point. The Standby mode is the third kind of low power mode besides CPU mode and set point, it is related to state of all CPU platform and has a much shorter transition time than setpoint. Only when all CPU platforms send standby request can the system can enter into standby mode.
This demo prints the power mode menu through the debug console, where the user can set the MCU to a specific power mode. User can wakeup the core by key interrupt. The purpose of this demo is to show how to switch between different power modes, and how to configure a wakeup source and wakeup the MCU from low power modes.
In chip PMIC board, DCDC is not used. PF5020’s SW1 output(1.1V) is connected to chip’s VDD_SOC_IN and SW2 output(1.8V) is connected to chip’s VDD_1P8_IN. PF5020’s ‘STANDBY’ pin is connected to PMIC_STBY_REQ.
Constraints with PMIC: 1.If the chip needs to enter STBY mode, just call the API and there is no more difference between internal DCDC and external PMIC. 2.If the chip doesn’t enter STBY mode, but will enter a low power mode, please pay attention to the DCDC output voltage of Current SP, Target SP and Wakeup SP. These voltage will be referred DCDC_C, DCDC_T and DCDC_W for short. 3.There are some constraints need to be met.
Low power mode without STBY – Enter a low power mode: 1.If DCDC_T > DCDC_C, increase DCDC voltage, switch SP, CPU mode switch 2.If DCDC_T < DCDC_C, switch SP, then decrease DCDC voltage, CPU mode switch 3.If DCDC_T = DCDC_C, switch SP, CPU mode switch
Low power mode without STBY – Wake up from a low power mode: 1.If DCDC_W > DCDC_T, CPU wake up, increase the DCDC voltage, switch SP 2.If DCDC_W < DCDC_T, CPU wake up, switch SP, decrease DCDC voltage 3.If DCDC_W = DCDC_T, CPU wake up, switch SP
Notes:
PMIC is controlled by LPI2C6, to make sure the clock supply for it. Using RC16M as the clock source and make sure the clock gate is enabled under any power mode.
No matter CM7 or CM4 as the main core, a synchronization mechanism are needed. The main core here is used to control the PMIC through LPI2C6, so that make sure the main core has been completed the steps that the lower power mode without STBY, then the other can enter or apply to it owns low power mode.
Tips: This demo is to show how the various power mode can switch to each other. However, in actual low power use case, to save energy and reduce the consumption even more, many things can be done including:
Disable the clock for unnecessary module during low power mode. That means, programmer can disable the clocks before entering the low power mode and re-enable them after exiting the low power mode when necessary.
Disable the function for unnecessary part of a module when other part would keep working in low power mode. At the most time, more powerful function means more power consumption. For example, disable the digital function for the unnecessary pin mux, and so on.
Set the proper pin state (direction and logic level) according to the actual application hardware. Otherwise, the pin current would be activated unexpectedly waste some energy.
Other low power consideration based on the actual application hardware.
Debug pins(e.g SWD_DIO) would consume addtional power, had better to disable related pins or disconnect them.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
USB to Com Converter
Board settings
To use EXT PMIC, Please do following Config Changes:
Change J41/J53/J67/J68/J69 Jumper Setting from 1-2 to 2-3
Change J71/J73/J19 Jumper Setting from 1-2 to OPEN
Change J72/J74/J77 Jumper Setting from OPEN to 1-2
DNP R1851,R1853 Populate R1852,R1854
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When running the demo, the debug console shows the menu to provide the desired operation. Here we take multicore targets as an example.
This is core0. Copy Secondary core image to address: 0x20200000, size: XXXXX Starting secondary core. The secondary core application has been started.
CPU wakeup source 0x10001…
Power Mode Switch Demo for iMXRT1176
Core0 send message to core1.
System previous setpoint is 0 System current setpoint is 0 M7 previous CPU mode is RUN M7 current CPU mode is RUN M7 CLK is 696 MHz M4 previous CPU mode is RUN M4 current CPU mode is RUN M4 CLK is 240 MHz
Please select the desired operation: Press A to demonstrate typical set point transition. Press B to demonstrate cpu mode switch in setpoint 0. Press C to enter SNVS mode.
Waiting for select…
When ‘A’ is selected, the menu shows selections for setpoint and CPU mode combination. If CPU enters SUSPEND mode, system will wake up from reset when wakeup event happening. Note: When user select F or G, CPU will be forced to enter SUSPEND mode since power domain WAKEUPMIX is off at setpoint 11~15. System will wake up from reset when wakeup event happening.
Set Point Transition: Press A to enter Set Point: 1 M7 CPU mode: RUN M4 CPU mode: RUN Press B to enter Set Point: 0 M7 CPU mode: RUN M4 CPU mode: RUN Press C to enter Set Point: 5 M7 CPU mode: RUN M4 CPU mode: RUN Press D to enter Set Point: 7 M7 CPU mode: RUN M4 CPU mode: STOP Press E to enter Set Point: 9 M7 CPU mode: STOP M4 CPU mode: RUN Press F to enter Set Point: 11 M7 CPU mode: SUSPEND M4 CPU mode: RUN Press G to enter Set Point: 12 M7 CPU mode: SUSPEND M4 CPU mode: RUN Press H to enter Set Point: 1 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press I to enter Set Point: 0 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press J to enter Set Point: 5 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press K to enter Set Point: 7 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press L to enter Set Point: 10 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press M to enter Set Point: 11 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press N to enter Set Point: 15 M7 CPU mode: SUSPEND M4 CPU mode: SUSPEND System standby Press ‘Q’ to exit
Waiting for select…
When ‘B’ is selected, the menu shows selections for different CPU mode with/without system standby request in setpoint0. If CPU enters SUSPEND mode, system will wake up from reset when wakeup event happening.
Cpu mode switch: Press A to enter cpu mode RUN Press B to enter cpu mode WAIT Press C to enter cpu mode STOP Press D to enter cpu mode SUSPEND Press E to enter cpu mode WAIT, system standby Press F to enter cpu mode STOP, system standby Press G to enter cpu mode SUSPEND, system standby Press ‘Q’ to exit
Waiting for select…
When ‘C’ is selected, the menu shows wake up source selection for SNVS mode.
Select the wake up source: Press T for Timer Press S for switch/button SW7.
Waiting for key press..
Note: In this application, DCDC will be turned off durig SP11~SP15. All memories and peripherals in CM7 platform and WAKEUPMIX/DISPLAYMIX/MEGAMIX will be powered down in SP11~SP15. For ram targets(debug/release), application can’t wake up from SP11~SP15 since data in ram will be lost.
Note: To debug in external flash, following steps are needed:
Select the flash target and compile.
Set the SW1: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J11.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to external flash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
Note: Flexspi_nor_debug and Flexspi_nor_release targets on armgcc toolchain need to click SW4(reset button) to run cases after downloading the image.