Enabling Additional Edgefast Open Examples on M4 core for RT1170# Table of Contents Introduction IAR Create an M4 project Rearrange source files Rearrange project files Adjust project settings Delete function Arm GCC Create an M4 project Rearrange source files Rearrange project files Adjust project setting Delete function MDK Create an M4 project Rearrange source files Rearrange project files Adjust project settings Delete function Note