ecat_servo_motor#
Overview#
This example is a implementation of EtherCAT servo motor system which is compliance with CiA402 profile running on one core.
The example only support one motor with quadrature encoder.
Running the demo#
Note that this code CAN NOT be compiled directly. Please follow the steps below:
Generate the SSC source code
Download Slave Stack Code Tool(SSC Tool V5.13) from BECKHOFF official website and install it.
Create a new folder to save all files generated by SSC tool.
Open Slave Stack Code Tool.
Click ‘File’ -> ‘New’ -> ‘Import’ to import the Congfig file.
Select servo_motor.xml under the path: “\boards<board>\ecat_examples\servo_motor<core>\SSC”. Click ‘Custom’ -> ‘NXP ECAT…’ -> ‘OK’ to select the subdevice description file
Click ‘File’ -> ‘Save’ to save the project to the new folder.
Click ‘Project’ -> ‘Create new Slave Files’.
Select ‘Source Folder’ to the new folder.Click ‘Start’.
The ESI file and SSC source code is saved on the new folder.
Copy SSC souce code to the mcuxsdk folder
Delete the “Src” folder under the path: “
\boards<board>\ecat_examples\servo_motor<core>\SSC’ Copy the whole “Src” folder in the new folder to “
\boards<board>\ecat_examples\servo_motor<core>\SSC’
Apply the patch
Change working directory to “\boards<board>\ecat_examples\servo_motor<core>\SSC”. Linux:
Download dos2unix command
apt-get install dos2unixTransfer SSC source code format
dos2unix Src/*Apply patch
patch -d ./ -p1 -i ./CiA402-combine-the-SSC-slave-with-ec_pmsm-support.patch
Windows:
Download patch.exe and Unix2Dos.exe tool
Download Windows Patch Utility from http://gnuwin32.sourceforge.net/downlinks/patch-bin-zip.php .
Download Dos2Unix/Unix2Dos-Text file format converters from https://sourceforge.net/projects/dos2unix/ .Transfer the patch format
$(Dos2Unix/Unix2Dos-DIR)/bin/unix2dos.exe CiA402-combine-the-SSC-slave-with-ec_pmsm-support.patchApply patch
patch.exe -d ./ -p1 -i ./CiA402-combine-the-SSC-slave-with-ec_pmsm-support.patch
After compilation and image download, the serial console will output:
Start the SSC servo_motor example...
Now this servo system is ready to wait EtherCAT MainDevice connection.
TwinCAT Setup#
To demonstrate this servo system, TwinCAT is used as the EtherCAT MainDevice.