MCUXpresso SDK Documentation

lwip_dhcp_enet_qos_bm

lwip_dhcp_enet_qos_bm#

Overview#

The lwip_dhcp demo application demonstrates a DHCP demo on the lwIP TCP/IP stack. The application acts as a DHCP client and prints the status as it is progressing. Once the interface is being bound to an IP address obtained from DHCP server, address information is printed.

Supported Boards#

MIMXRT1170-EVKB
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1170-EVKB board

  • Personal Computer

Board settings

No special settings are required.

FRDM-IMXRT1152
Hardware requirements
  • FRDM-IMXRT1152 board

  • USB Type-C cable

  • RJ45 network cable

  • Personal Computer

Board settings
  • Connect the USB Type-C cable to the FRDM-IMXRT1152 USB debug connector.

  • Use the 10/100 Ethernet RJ45 port (J55).

  • Set JP2 to position 1-2.

FRDM-MCXE32B
Hardware requirements
  • USB-C cable

  • Network cable RJ45 standard

  • FRDM-MCXE32B board

  • Personal Computer

Board settings

No special settings are required.

MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • Network cable RJ45 standard

  • MCIMX93-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J501) as default.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • Network cable RJ45 standard

  • MCIMX93W-EVK board

  • Personal Computer

Board settings

This example uses 1G port(J501) as default.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • MCIMX93-QSB board

  • Personal Computer

Board settings

No special settings are required.

Note

Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.

FRDM-MCXE31B
Hardware requirements
  • USB-C cable

  • Network cable RJ45 standard

  • FRDM-MCXE31B board

  • Personal Computer

Board settings

No special settings are required.

MIMXRT2660-EVK
Hardware requirements
  • USB Type-C cable for debug console

  • Network cable RJ45 standard

  • MIMXRT2660-EVK board

  • Personal Computer

Board settings

This example uses the on-board COMM_ENET_QOS port (gigabit YT8531 PHY, RGMII), which terminates at RJ45 port J57. Set jumper J52 pins 2-3 to route the on-board analog mux to the external RGMII PHY before running the example.

10BASE-T1S PHY support

This example supports the internal 10BASE-T1S PHY (TENBASET_PHY) as an alternative to the external RGMII PHY. To enable, define in board.h:

#define BOARD_NETWORK_USE_TENBASET_PHY (1U)

Hardware setup for 10BASE-T1S mode:

  • Set jumper J52 to position 1-2 to route the board analog mux to the T1S PHY.

  • Attach the T1S link to RJ45 port J40 (the T1S connector dedicated to COMM_ENET_QOS on this EVK).

Hardware setup for RGMII mode:

  • Set jumper J52 to position 2-3 to route the board analog mux to the external RGMII PHY.

  • Use RJ45 port J57 for the RGMII link.