lwip_dhcp_enet_qos_freertos#
Overview#
The lwip_dhcp demo application demonstrates a DHCP demo on the lwIP TCP/IP stack. The application acts as a DHCP client and prints the status as it is progressing. Once the interface is being bound to an IP address obtained from DHCP server, address information is printed.
Supported Boards#
MIMXRT1170-EVKB
Hardware requirements
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Board settings
No special settings are required.
FRDM-IMXRT1152
Hardware requirements
FRDM-IMXRT1152 board
USB Type-C cable
RJ45 network cable
Personal Computer
Board settings
Connect the USB Type-C cable to the FRDM-IMXRT1152 USB debug connector.
Use the 10/100 Ethernet RJ45 port (J55).
Set JP2 to position 1-2.
FRDM-MCXE32B
Hardware requirements
USB-C cable
Network cable RJ45 standard
FRDM-MCXE32B board
Personal Computer
Board settings
No special settings are required.
MCIMX93-EVK
Hardware requirements
USB Type-C cable
Network cable RJ45 standard
MCIMX93-EVK board
Personal Computer
Board settings
This example uses 1G port(J501) as default.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
MCIMX93W-EVK
Hardware requirements
USB Type-C cable
Network cable RJ45 standard
MCIMX93W-EVK board
Personal Computer
Board settings
This example uses 1G port(J501) as default.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
MCIMX93-QSB
Hardware requirements
USB Type-C cable
MCIMX93-QSB board
Personal Computer
Board settings
No special settings are required.
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
FRDM-MCXE31B
Hardware requirements
USB-C cable
Network cable RJ45 standard
FRDM-MCXE31B board
Personal Computer
Board settings
No special settings are required.
MIMXRT2660-EVK
Hardware requirements
USB Type-C cable for debug console
Network cable RJ45 standard
MIMXRT2660-EVK board
Personal Computer
Board settings
This example uses the on-board COMM_ENET_QOS port (gigabit YT8531 PHY, RGMII), which terminates at RJ45 port J57. Set jumper J52 pins 2-3 to route the on-board analog mux to the external RGMII PHY before running the example.
10BASE-T1S PHY support
This example supports the internal 10BASE-T1S PHY (TENBASET_PHY) as an alternative to the external RGMII PHY. To enable, define in board.h:
#define BOARD_NETWORK_USE_TENBASET_PHY (1U)
Hardware setup for 10BASE-T1S mode:
Set jumper J52 to position 1-2 to route the board analog mux to the T1S PHY.
Attach the T1S link to RJ45 port J40 (the T1S connector dedicated to COMM_ENET_QOS on this EVK).
Hardware setup for RGMII mode:
Set jumper J52 to position 2-3 to route the board analog mux to the external RGMII PHY.
Use RJ45 port J57 for the RGMII link.