Symmetric key algorithm based Initial Attestation#
- Author:
David Hu
- Organization:
Arm Limited
- Contact:
Introduction#
This document proposes a design of symmetric key algorithm based Initial Attestation in TF-M.
Symmetric key algorithm based Initial Attestation (symmetric Initial Attestation for short) signs and verifies Initial Attestation Token (IAT) with a symmetric cryptography signature scheme, such as HMAC. It can reduce TF-M binary size and memory footprint on ultra-constrained devices without integrating asymmetric ciphers.
This proposal follows PSA Attestation API document 1PSA Attestation API 1.0 (ARM IHI 0085).
Note
As pointed out by PSA Attestation API [1], the use cases of Initial Attestation based on symmetric key algorithms can be limited due to the associated infrastructure costs for key management and operational complexities. It may also restrict the ability to interoperate with scenarios that involve third parties.
Design overview#
The symmetric Initial Attestation follows the existing IAT generation sequence for Initial Attestation based on asymmetric key algorithm (asymmetric Initial Attestation for short).
As Profile Small design 2Trusted Firmware-M Profile Small Design requests, a configuration flag
SYMMETRIC_INITIAL_ATTESTATION selects symmetric initial attestation during
build.
The top-level design is shown in Overall design diagram below.
Overall design diagram#
Symmetric Initial Attestation adds its own implementations of some steps in IAT generation in Initial Attestation secure service. More details are covered in IAT generation in Initial Attestation secure service.
The interfaces and procedures of Initial Attestation secure service are not affected. Refer to Initial Attestation Service Integration Guide 3Initial Attestation Service Integration Guide for details of the implementation of Initial Attestation secure service.
Symmetric Initial Attestation invokes t_cose library to build up
COSE_Mac0 structure.
COSE_Mac0 support is added to t_cose library in TF-M since official
t_cose hasn’t supported COSE_Mac0 yet. The design of COSE_Mac0
support is covered in COSE_Mac0 support in t_cose.
Note
The COSE_Mac0 implementation in this proposal is a prototype only for
Proof of Concept so far. It may be replaced after t_cose officially
supports COSE_Mac0 message.
Several HAL APIs are defined to fetch platform specific assets required by
Symmetric Initial Attestation. For example, tfm_plat_get_symmetric_iak()
fetches symmetric Initial Attestation Key (IAK). Those HAL APIs are summarized
in HAL APIs.
Decoding and verification of symmetric Initial Attestation is also included in this proposal for regression test. The test suites and IAT decoding are discussed in TF-M Test suite.
QCBOR library and Crypto service are also invoked. But this proposal doesn’t
require any modification to either QCBOR or Crypto service. Therefore,
descriptions of QCBOR and Crypto service are skipped in this document.
IAT generation in Initial Attestation secure service#
The sequence of IAT generation of symmetric Initial Attestation is shown in
Symmetric IAT generation flow in Initial Attestation secure service below. Note that the Register symmetric IAK stage
is no longer required due to changes in the Crypto partition
(attest_symmetric_key.c is now responsible only for calculating the instance
ID).
Symmetric IAT generation flow in Initial Attestation secure service#
In Initial Attestation secure service, symmetric Initial Attestation implements
the following steps in attest_create_token(), which are different from those
of asymmetric Initial Attestation.
attest_token_start()Instance ID claims
attest_token_finish()
If SYMMETRIC_INITIAL_ATTESTATION is selected, symmetric Initial Attestation
dedicated implementations of those steps are included in build.
Otherwise, asymmetric Initial Attestation dedicated implementations are included
instead.
Symmetric Initial Attestation implementation resides a new file
attest_symmetric_key.c to handle symmetric Instance ID related operations.
Symmetric Initial Attestation dedicated attest_token_start() and
attest_token_finish() are added in attestation_token.c.
The details are covered in following sections.
Symmetric Instance ID#
Symmetric Initial Attestation dedicated attest_symmetric_key.c implements
the attest_get_instance_id() function. This function returns the Instance ID
value, calculating it if it has not already been calculated. Refer to
Instance ID claim_ for more details.
Note
Only symmetric IAK for HMAC algorithm is allowed so far.
Instance ID calculation#
In symmetric Initial Attestation, Instance ID is also calculated the first time it is requested. It can protect critical symmetric IAK from being frequently fetched, which increases the risk of asset disclosure.
The Instance ID value is the output of hashing symmetric IAK raw data twice, as requested in PSA Attestation API [1]. HMAC-SHA256 may be hard-coded as the hash algorithm of Instance ID calculation.
4HMAC: Keyed-Hashing for Message AuthenticationNote
According to RFC2104 4HMAC: Keyed-Hashing for Message Authentication, if a HMAC key is longer than the HMAC block size, the key will be first hashed. The hash output is used as the key in HMAC computation.
In current design, HMAC is used to calculate the authentication tag of
COSE_Mac0. Assume that symmetric IAK is longer than HMAC block size
(HMAC-SHA256 by default), the Instance ID is actually the HMAC key for
COSE_Mac0 authentication tag generation, if Instance ID value is the
output of hashing IAK only once.
Therefore, attackers may request an valid IAT from device and fake malicious
ones by using Instance ID to calculate valid authentication tags, to cheat
others.
As a result, symmetric IAK raw data should be hashed twice to generate the Instance ID value.
The Instance ID calculation result is stored in a static buffer.
Token generation process can call attest_get_instance_id() to
fetch the data from that static buffer.
attest_token_start()#
Symmetric Initial Attestation dedicated attest_token_start() initializes the
COSE_Mac0 signing context and builds up the COSE_Mac0 Header.
The workflow inside attest_token_start() is shown in
Workflow in symmetric Initial Attestation attest_token_start() below.
Workflow in symmetric Initial Attestation attest_token_start()#
Descriptions of each step are listed below:
t_cose_mac0_sign_init()is invoked to initializeCOSE_Mac0signing context int_cose.The symmetric IAK handle is set into
COSE_Mac0signing context viat_cose_mac0_set_signing_key().Initialize
QCBORencoder.The header parameters are encoded into
COSE_Mac0structure int_cose_mac0_encode_parameters().QCBOREncode_OpenMap()prepares for encoding theCOSE_Mac0payload, which is filled with IAT claims.
All the COSE_Mac0 functionalities in t_cose are covered in
COSE_Mac0 support in t_cose.
Instance ID claim#
Symmetric Initial Attestation also implements Instance ID claims in
attest_add_instance_id_claim().
The Instance ID value is fetched via attest_get_instance_id().
The value has already been calculated during symmetric IAK registration. See
Instance ID calculation for details.
The other steps are the same as those in asymmetric Initial Attestation implementation. The UEID type byte is set to 0x01.
attest_token_finish()#
Symmetric Initial Attestation dedicated attest_token_finish() calls
t_cose_mac0_encode_tag() to calculate and encode the authentication tag of
COSE_Mac0 structure.
The whole COSE and CBOR encoding are completed in attest_token_finish().
The simplified flow in attest_token_finish() is shown in
Workflow in symmetric Initial Attestation attest_token_finish() below.
Workflow in symmetric Initial Attestation attest_token_finish()#
COSE_Mac0 support in t_cose#
COSE_Mac0 supports in t_cose in TF-M include the following major
functionalities:
Encoding
COSE_Mac0structureDecoding and verifying
COSE_Mac0structureHMAC computation to generate and verify authentication tag
Short-circuit tagging for test mode
According to RFC8152 5CBOR Object Signing and Encryption (COSE), COSE_Mac0 and COSE_Sign1 have similar
structures. Therefore, the prototype follows COSE_Sign1 implementation to
build up COSE_Mac0 file structure and implement COSE_Mac0 encoding and
decoding.
Although COSE_Mac0 can share lots of data types, APIs and encoding/decoding
steps with COSE_Sign1 in implementation, this prototype separates
COSE_Mac0 implementation from COSE_Sign1. COSE_Mac0 owns its
dedicated signing/verification contexts, APIs and encoding/decoding process.
The purposes of separating COSE_Mac0 and COSE_Sign1 are listed below
It can keep changes to
COSE_Sign1as small as possible and avoid conflicts with development inCOSE_Sign1`. It can decrease conflicts ift_cosein TF-M is synchronized with originalt_coserepository later.COSE_Mac0andCOSE_Sign1are exclusive in TF-M use cases. It cannot decrease TF-M memory footprint by extracting the common components shared byCOSE_Mac0andCOSE_Sign1but can make the design over-complicated.
Note
Only HMAC is supported in current COSE_Mac0 prototype.
File structure#
New files are added to implement the functionalities listed above. The structure of files is shown in the table below.
Directory |
Files |
Descriptions |
|---|---|---|
|
|
Encode |
|
Decode and verify |
|
|
|
Data type definitions and function
declarations of encoding and signing
|
|
Data type definitions and function
declarations of verifying |
Other t_cose files may also be changed to add COSE_Mac0 associated data
types and function declarations.
HMAC operations are added in crypto_adapters/t_cose_psa_crypto.c.
Preprocessor flags are added to select corresponding crypto for COSE message
signing and verification.
T_COSE_ENABLE_SIGN1selects ECDSA and Hash operations forCOSE_Sign1.
T_COSE_ENABLE_MAC0selects HMAC operations forCOSE_Mac0.
Encoding COSE_Mac0#
Following COSE_Sign1 implementation, COSE_Mac0 encoding exports similar
functions to Initial Attestation secure service.
The major functions are listed below.
Initialize signing context#
t_cose_mac0_sign_init() initializes COSE_Mac0 signing context and
configures option flags and algorithm used in signing.
static void
t_cose_mac0_sign_init(struct t_cose_mac0_sign_ctx *me,
int32_t option_flags,
int32_t cose_algorithm_id);
The COSE_Mac0 signing context is defined as
struct t_cose_mac0_sign_ctx {
/* Private data structure */
uint8_t protected_parameters_buffer[
T_COSE_MAC0_MAX_SIZE_PROTECTED_PARAMETERS];
struct q_useful_buf_c protected_parameters; /* The encoded protected parameters */
int32_t cose_algorithm_id;
struct t_cose_key signing_key;
int32_t option_flags;
struct q_useful_buf_c kid;
...
};
Set signing key#
t_cose_mac0_set_signing_key() sets the key used in COSE_Mac0 signing.
Optional kid, as a key identifer, will be encoded into COSE_Mac0 Header
unprotected bucket.
static void
t_cose_mac0_set_signing_key(struct t_cose_mac0_sign_ctx *me,
struct t_cose_key signing_key,
struct q_useful_buf_c kid);
Encode Header parameters#
t_cose_mac0_encode_parameters() encodes the COSE_Mac0 Header parameters
and outputs the encoded context to cbor_encode_ctx.
enum t_cose_err_t
t_cose_mac0_encode_parameters(struct t_cose_mac0_sign_ctx *context,
QCBOREncodeContext *cbor_encode_ctx);
Calculate and add authentication tag#
t_cose_mac0_encode_tag() calculates the authentication tag and finishes the
COSE_Mac0 message.
enum t_cose_err_t
t_cose_mac0_encode_tag(struct t_cose_mac0_sign_ctx *context,
QCBOREncodeContext *cbor_encode_ctx);
Decoding COSE_Mac0#
Following COSE_Sign1 implementation, COSE_Mac0 decoding exports similar
functions to test suite of Initial Attestation.
The major functions are listed below.
Initialize verification context#
t_cose_mac0_verify_init() initializes COSE_Mac0 verification context and
configures option flags in verification.
static void
t_cose_mac0_verify_init(struct t_cose_mac0_verify_ctx *context,
int32_t option_flags);
The COSE_Mac0 verification context is defined as
struct t_cose_mac0_verify_ctx {
/* Private data structure */
struct t_cose_key verification_key;
int32_t option_flags;
};
Set verification key#
t_cose_mac0_set_verify_key() sets the key for verifying COSE_Mac0
authentication tag.
static void
t_cose_mac0_set_verify_key(struct t_cose_mac0_verify_ctx *context,
struct t_cose_key verify_key);
Decode and verify COSE_Mac0#
t_cose_mac0_verify() decodes the COSE_Mac0 structure and verifies the
authentication tag.
enum t_cose_err_t
t_cose_mac0_verify(struct t_cose_mac0_verify_ctx *context,
struct q_useful_buf_c cose_mac0,
struct q_useful_buf_c *payload,
struct t_cose_parameters *parameters);
Short-circuit tagging#
If T_COSE_OPT_SHORT_CIRCUIT_TAG option is enabled, COSE_Mac0 encoding
will hash the COSE_Mac0 content and add the hash output as an authentication
tag. It is useful when critical symmetric IAK is unavailable or cannot be
accessed, perhaps because it has not been provisioned or configured for the
particular device. It is only for test and must not be used in actual use case.
The kid parameter will either be skipped in COSE_Mac0 Header.
If T_COSE_OPT_ALLOW_SHORT_CIRCUIT option is enabled, COSE_Mac0 decoding
will only verify the hash output, without requiring symmetric key for
authentication tag verification.
TF-M Test suite#
Symmetric Initial Attestation adds dedicated non-secure and secure test suites.
The test suites also follow asymmetric Initial Attestation test suites
implementation but optimize the memory footprint.
Symmetric Initial Attestation non-secure and secure test suites request Initial
Attestation secure service to generate IATs. After IATs are generated
successfully, test suites decode IATs and parse the claims.
Secure test suite also verifies the authentication tag in COSE_Mac0
structure.
Symmetric Initial Attestation implements its dedicated
attest_token_decode_validate_token() in attest_symmetric_iat_decoded.c
to perform IAT decoding required by test suites.
If SYMMETRIC_INITIAL_ATTESTATION is selected,
attest_symmetric_iat_decoded.c is included in build.
Otherwise, asymmetric Initial Attestation dedicated implementations are included
instead.
The workflow of symmetric Initial Attestation dedicated
attest_token_decode_validate_token() is shown below.
Workflow in symmetric Initial Attestation attest_token_decode_validate_token()#
If the decoding is required from secure test suite,
attest_token_decode_validate_token() will fetch symmetric IAK to verify the
authentication tag in COSE_Mac0 structure.
If the decoding is required from non-secure test suite,
attest_token_decode_validate_token() will decode COSE_Mac0 only by
setting T_COSE_OPT_DECODE_ONLY option flag. Non-secure must not access the
symmetric IAK.
HAL APIs#
HAL APIs are summarized below.
Fetch device symmetric IAK#
tfm_plat_get_symmetric_iak() fetches device symmetric IAK.
enum tfm_plat_err_t tfm_plat_get_symmetric_iak(uint8_t *key_buf, size_t buf_len, size_t *key_len, psa_algorithm_t *key_alg);Parameters:
key_bufBuffer to store the symmetric IAK.
buf_lenThe length of
key_buf.
key_lenThe length of the symmetric IAK.
key_algThe key algorithm. Only HMAC SHA-256 is supported so far.
It returns error code specified in enum tfm_plat_err_t.
Get symmetric IAK key identifier#
attest_plat_get_symmetric_iak_id() gets the key identifier of the symmetric
IAK as the kid parameter in COSE Header.
Optional if device doesn’t install a key identifier for symmetric IAK.
enum tfm_plat_err_t attest_plat_get_symmetric_iak_id(void *kid_buf, size_t buf_len, size_t *kid_len);Parameters:
kid_bufBuffer to store the IAK identifier.
buf_lenThe length of
kid_buf.
kid_lenThe length of the IAK identifier.
It returns error code specified in enum tfm_plat_err_t.
Reference#
Copyright (c) 2020-2022 Arm Limited. All Rights Reserved.