TF-M Crypto Service design#
- Author:
Antonio de Angelis
- Organization:
Arm Limited
- Contact:
Antonio de Angelis <antonio.deangelis@arm.com>
Abstract#
This document describes the design of the TF-M Cryptographic Secure Service (in short, TF-M Crypto service).
Introduction#
The TF-M Crypto service provides an implementation of the PSA Certified Crypto
APIs in a PSA RoT secure partition in TF-M. It is based on the Mbed TLS
project, which provides a reference implementation of the PSA Crypto APIs as a
C software library. For more details on the PSA Crypto APIs refer to 1PSA Certified Crypto API specifications: https://arm-software.github.io/psa-api/crypto/,
while for the Mbed TLS reference software refer to 2Using PSA - Getting started in Mbed TLS: https://mbed-tls.readthedocs.io/en/latest/getting_started/psa/ and 3Mbed TLS repository which holds the reference implementation as a C software library: Mbed-TLS
The service can be requested by other services running in the SPE, or by applications running in the NSPE, and its aim is to provide cryptographic primitives in a secure and efficient way, either via software or by routing the calls to any underlying crypto hardware accelerator or secure element that the platform might provide.
Components#
The TF-M Crypto service is implemented by a number of different firmware components residing in the Crypto partition, which are listed below:
Component name |
Description |
Location |
|---|---|---|
Client API interface |
This module exports the PSA Crypto API to be callable from the users, which are called also clients. They could be either other secure partitions or Non Secure world based callers. |
|
Mbed TLS |
The Mbed TLS |
Needed as dependency specified by the |
Init module |
This module handles the initialisation of the service objects during TF-M boot and provides the infrastructure to service requests when TF-M is built for IPC or SFN model. The dispatching mechanism of IPC requests is based on a look up table of function pointers. This design allows for better scalability and support of a higher number of Secure functions with minimal overhead and duplication of code. This module is in charge of providing an ID of the caller of each API in the backend, allowing to enforce key ownership policies. |
|
Alloc module |
This module handles the allocation of contexts for multipart
operations in the Secure world. This is required because the
caller view of contexts, i.e. clients, does not contain any
sensible information but just a number handle which is then
used by the service itself to match the context to the actual
context information which will be stored securely in the TF-M
crypto partition private memory. This is enabled by setting
|
|
Service modules |
These modules (AEAD, Asymmetric, Cipher, Hash, Key Derivation, Key Management, MAC, Random Number Generation) represent a thin layer which is in charge of servicing the calls from the clients. They provide parameter sanitization and context retrieval for multipart operations, and dispatching to the corresponding backend library function exposed by the underlying library. |
|
Backend library abstraction |
This module contains several APIs to abstract the interface towards the backend library, which must provide the PSA Crypto core layer, key management, SW based crypto and possibly interfaces for HW crypto accelerators and Secure Elements |
|
Manifest |
The manifest file is a description of the service components. |
|
CMake, Kconfig and headers |
The CMake files are used by the TF-M CMake build system to
build the service as part of the Secure FW build. The service
is built as a static library
( |
|
TF-M Crypto key abstraction |
The TF-M Crypto service has its own type definition to be able
to identify a key ID with its own owner. The definition of an
owner is provided by the TF-M Firmware Framework and is out of
the scope of the service itself and the PSA Crypto APIs spec.
The underlying library in practice must provide the same
functionality, i.e handle key IDs with associated owner info.
For Mbed TLS, this is accomplished by the type
|
|
Documentation |
The integration guide contains the description of the TF-M Crypto service modules and interfaces. |
|
The interaction between the different components is described by the
block diagram in block_diagram-label
Block diagram of the firmware architecture of the TF-M Crypto service. Dotted
lines between services represent isolation boundaries once runtime firmware
is initialized, i.e. TF-M init phase has completed. The diagram is simplified
and shows only the major functional blocks, for a more detailed
libmbedcrypto.a architecture please refer to [3].#
Relationship between Mbed TLS and the TF-M Crypto service#
TF-M Crypto as a particular configuration of Mbed TLS#
Up until TF-Mv2.0, the TF-M Crypto service used to provide its own separate implementation of the PSA Certified Crypto APIs, i.e. it provided its own version of the implementation defined aspects of the specifications. Starting from TF-Mv2.1, the TF-M Crypto service fully aligns to the implementation defined by the Mbed TLS project, i.e. its implementation defined aspects are the same as the ones defined by Mbed TLS.
As a consequence, starting from TF-Mv2.1 the PSA Crypto headers available in TF-M are a copy of those distributed by the Mbed TLS project. TF-M just uses them and won’t accept any contribution to them, as those need to be discussed in the scope of the Mbed TLS project.
TF-M then represents just a configuration of the Mbed TLS reference
implementation where the TF-M Crypto APIs are provided as a remote call across
a transport channel, which might be represented by a TrustZone boundary (in
Armv8.x-M systems), by a mailbox channel in heterogeneous systems, e.g. Cortex-A
+ Cortex-M systems, by an SPM mediated interface, e.g. partition to partition
calls or, in general, through a mechanism which provides process separation
between the client and the service sides of the API.
In this context, the client must always define the Mbed TLS config option
MBEDTLS_PSA_CRYPTO_CLIENT, while the service must always have
MBEDTLS_PSA_CRYPTO_SPM, mainly to avoid symbol clashing at link time between
the library interface and the tfm_crypto_api.c interface. When there is a
component on the service side which is able to identify the client through an
ID, it is recommended to also define MBEDTLS_PSA_CRYPTO_KEY_ID_ENCODES_OWNER
option in order to provide separation in the key space.
Usage of Mbed TLS configuration headers#
Mbed TLS uses two different configuration headers, specified through the setting
of the MBEDTLS_CONFIG_FILE, i.e. Mbed TLS config, and the setting of
MBEDTLS_PSA_CRYPTO_CONFIG_FILE, i.e. the PSA configuration. In order to be
able to perform header inclusion for psa/crypto.h, the configuration files
must be visible to the compilation unit through the include hierarchy. If none of
the macros are defined, the fall back strategy is to include the default config
files available in the Mbed TLS repo, i.e. include/mbedtls/mbedtls_config.h
and include/psa/crypto_config.h, which contain a set of default values for
the macros.
Usage of the default header config when using the TF-M Crypto service is highly
discouraged, mainly because both on the client side and on the service side a
set of options must always be defined (or undefined), as described in the
previous section. TF-M provides example _profiles_ which show the options and
how they should be used on both client and service side of the integration. Note
that to avoid falling back to the default PSA configuration, the Mbed TLS config
file must always define the symbol MBEDTLS_PSA_CRYPTO_CONFIG. The symbol to
enable the Mbed TLS config MBEDTLS_CONFIG_FILE instead must be available to
the unit being compiled which is including psa/crypto.h, i.e. passed by the
build system config stage.
Hardware acceleration#
The TF-M Crypto partition must handle all HW related crypto tasks, if the platform is capable of offering hardware acceleration or if a complete Secure Element is present. The main difference between the two is that a hardware accelerator does not store keys but just accelerates operations, while a Secure Element is capable of storing keys and the PSA Crypto core running on the host must interface with it to store, retrieve or use them for crypto tasks, etc.
There are currently two methods to interface an accelerator into the Crypto service, and both rely on the Crypto partition fully owning the Crypto hardware, i.e. the memory mapped IO space must be bound the Crypto partition only. Both methods are implemented through the capability of the _backend_ library to either:
Provide a link time mechanism to replace pure SW implementations for algorithms with HW assisted implementations. In this case, the TF-M platform provides some additional HW abstraction through the usage of
crypto_hw_accelerator_*()APIs. This is dubbed the _ALT approach and will be soon to be deprecated potentially starting from the release of Mbed TLS 4.0
4PSA Unified Driver Interface for Cryptoprocessors: Mbed-TLS/mbedtlsProvide a cleanly defined interface specification 4PSA Unified Driver Interface for Cryptoprocessors: Mbed-TLS/mbedtls to describe the APIs that a driver must expose to the PSA Crypto core in order for the core to be able to offload operations to hardware. This is the preferred method for interfacing with HW.
Both solutions are currently handled at build time (either compilation or linking) by Mbed TLS. For details on how to integrate a driver please refer directly to the documentation referenced above and to the Mbed TLS repo.
Builtin keys#
A particular driver using the interface described in [4] is the TF-M Builtin
Key Loader driver 5TF-M Builtin Key Loader driver, normally described as tfm_builtin_key_loader. The goal of the driver is to make Mbed TLS aware of
transparent builtin keys, i.e. keys which can be read from the core (i.e. not
fully opaque keys), but that are normally bound to the platform and provisioned
in it, for which it would be more appropriate to treat them as standard
transparent keys. The concept of transparent builtin keys is not defined
in the spec so it is specifically a non standard extension added by TF-M to the
Mbed TLS implementation, which might be changed between releases until a standard
solution is adopted. TF-M patches Mbed TLS on the fly to enable such behaviour
using patches available in lib/ext/mbedcrypto. Implementations might disable
the tfm_builtin_key_loader and then must provide their own alternative storage
location for all of the TF-M required builtin keys, e.g. by having them stored in
a Secure Element with a corresponding opaque driver.
Service API description#
The Alloc and Init modules implement public APIs which are specific to
the TF-M Crypto service, and are available only internally to other components
of the TF-M Crypto partition. For a detailed description of the prototypes
please refer to the tfm_crypto_api.h header.
Function |
Module |
Caller |
Scope |
|---|---|---|---|
tfm_crypto_init() |
Init |
SPM |
Called during TF-M boot for initialisation. It does modules initialisation (it initializes the Alloc module) and initializes the backend library. Being the partition enabled for the SFN model, it does not implement any IPC specific message handler, instead it relies on the SPM being able to schedule SFN partitions using the SFN dispatcher with little overhead |
tfm_crypto_sfn() |
Init |
SPM |
Function to handle an SFN request or to interface with the message handler when running in IPC model |
tfm_crypto_init_alloc() |
Alloc |
Init |
Called by |
tfm_crypto_operation_alloc() |
Alloc |
Service modules |
It allocates a new operation context for a multipart operation. It returns an handle to the allocated context in secure memory. |
tfm_crypto_operation_lookup() |
Alloc |
Service modules |
It retrieves a previously allocated operation context of a multipart operation, based on the handle given as input. |
tfm_crypto_operation_release() |
Alloc |
Service modules |
It releases a previously allocated operation context of a multipart operation, based on the handle given as input. |
tfm_crypto_*_interface() |
|
Init |
Interface functions called by the dispatcher to service PSA Crypto APIs requests |
Configuration parameters#
The TF-M Crypto service exposes some configuration parameters to tailor the service configuration in terms of supported functionalities and hence FLASH/RAM size to meet the requirements of different platforms and use cases. These parameters can be provided via CMake parameters during the CMake configuration step and as a configuration header to allow the configuration of the Mbed TLS library. When using Kconfig they are also exported in the Kconfig menus.
Parameter |
Type |
Description |
Default |
|---|---|---|---|
CRYPTO_ENGINE_BUF_SIZE |
CMake build configuration parameter |
Buffer used by Mbed TLS for its own allocations at runtime. This is a buffer allocated in static memory. |
8096 (bytes) |
CRYPTO_CONC_OPER_NUM |
CMake build configuration parameter |
This parameter defines the maximum number of possible concurrent operation contexts (cipher, MAC, hash and key deriv) for multi-part operations, that can be allocated simultaneously at any time. |
8 |
CRYPTO_IOVEC_BUFFER_SIZE |
CMake build configuration parameter |
This parameter applies only to IPC model builds. In IPC model, during a Service call, input and outputs are allocated temporarily in an internal scratch buffer whose size is determined by this parameter. |
5120 (bytes) |
CRYPTO_STACK_SIZE |
CMake build configuration parameter |
Defines the stack size assigned to the crypto partition in higher level of isolation configurations (L1 isolation has a common stack shared by all partitions) |
6912 (bytes) |
CRYPTO_NV_SEED |
CMake build configuration parameter |
Uses the Mbed TLS Crypto NV seed feature to provide entropy in case there is no HW acceleration providing HW entropy |
Defined for platforms which don’t have |
CRYPTO_IOVEC_BUFFER_SIZE |
CMake build configuration parameter |
Defines the size of scratch buffers to handle input/outputs if the Memory Mapped IOVEC feature is not enabled |
5120 (bytes) |
CRYPTO_SINGLE_PART_FUNCS_DISABLED |
CMake build configuration parameter |
When enabled, only the multipart, i.e. non-integrated APIs will be available in the service |
Not defined (Profile default) |
CRYPTO_*_MODULE_ENABLED |
CMake build configuration parameters |
When enabled, the correspoding shim layer module and relative APIs are available in the service |
Defined (Profile default) |
MBEDTLS_CONFIG_FILE |
Configuration header |
The Mbed TLS library can be configured to support different algorithms through the usage of a configuration header file at build time. This allows for tailoring FLASH/RAM requirements for different platforms and use cases. |
|
MBEDTLS_PSA_CRYPTO_CONFIG_FILE |
Configuration header |
This header file specifies which cryptographic mechanisms are available through the PSA API when MBEDTLS_PSA_CRYPTO_CONFIG is enabled, and is not used when MBEDTLS_PSA_CRYPTO_CONFIG is disabled. Configuring TF-M always involves having the define enabled. |
|
References#
Copyright (c) 2019-2024, Arm Limited. All rights reserved.