MCUXpresso SDK Documentation

Alignment notes

Alignment notes#

Source image alignment requirement

The buffer start address and stride byte-alignment requirement for a pixel depends on the specific pixel format and the gcFEATURE_VG_16PIXELS_ALIGNED value (0/1) in the vg_lite_options.h file.

|Image format|Bits per pixel|Start address alignment requirement in bytes|Stride alignment requirement in bytes

|Supported for source image|Supported for destination| |————|————–|——————————————–|—————————————|————————–|————————-| |VG_LITE_INDEX1|1|8B|8B|Yes| | |VG_LITE_INDEX2|2|8B|8B|Yes|| |VG_LITE_INDEX4|4|8B|8B|Yes|| |VG_LITE_INDEX8|8|16B|16B|Yes|| |VG_LITE_A4|4|4B|8B|Yes|| |VG_LITE_A8|8|4B|16B|Yes|Yes| |VG_LITE_L8|8|4B|16B|Yes|Yes| |VG_LITE_ARGB2222 group|8|4B|16B|Yes|Yes| |VG_LITE_RGB565 group|16|4B|32B|Yes|Yes| |VG_LITE_ARGB1555 group|16|4B|32B|Yes|Yes| |VG_LITE_ARGB4444 group|16|4B|32B|Yes|Yes| |VG_LITE_YUY2/UYVY|16|4B|32B|Yes|| |VG_LITE_ARGB8888/XRGB8888 group|32|4B|64B|Yes|Yes| |VG_LITE_ARGB8565/RGB888 group|32|4B|64B|Yes|Yes| |VG_LITE_NV12_TILED|Tile 4x4|Y: 16B

UV: 8B

|Y: 16B

UV: 8B

|Yes|| |VG_LITE_ANV12_TILED|Tile 4x4|Y: 16B

UV: 8B

|Y: 16B

UV: 8B

|Yes|| |VG_LITE_AYUY2_TILED|Tile 4x4|32B|32B|Yes||

VGLite hardware requires the raster image width to be a multiple of 16 pixels for linear gradient and radial gradient operations. This requirement applies to all image formats. Therefore, the user must pad an arbitrary image width to a multiple of 16 pixels for the VGLite linear gradient and radial gradient APIs.

Destination alignment requirement:

  • For Pixel Engine (PE) destination, the alignment should be 64B for all tiled (4x4) formats.

  • Alignment may also be limited by the alignment requirements of backend modules such as DC (Display Controller).

Parent topic:vg_lite_buffer_format_t enumeration