Blit structures#
This section provides details about blit structures.
vg_lite_buffer_t structure#
Defined under the “Pixel buffer structures” section (see vg_lite_buffer_t structure).
Parent topic:Blit structures
vg_lite_color_key_t structure#
A “color key” have two sections, where each section contains R,G,B channels, which are noted as high_rgb and low_rgb respectively. (from April 2022)
When the enable value is true, the color key specified is effective and the alpha value is used to replace the alpha channel of the destination pixel when its RGB channels are in range [low_rgb, high_rgb]. After the color key is used in the current frame, if the color key is not needed for the next frame, it should be disabled before the next frame.
Used in structure: vg_lite_color_key4_t
vg_lite_color_key_t members |
Type |
Description |
|---|---|---|
|
vg_lite_uint8_t |
When set (true), this color key is enabled |
|
vg_lite_uint8_t |
The R channel of |
|
vg_lite_uint8_t |
The G channel of |
|
vg_lite_uint8_t |
The B channel of |
|
vg_lite_uint8_t |
The alpha value to replace the destination pixel alpha channel value with |
|
vg_lite_uint8_t |
The R channel of |
|
vg_lite_uint8_t |
The G channel of |
|
vg_lite_uint8_t |
The B channel of |
Parent topic:Blit structures
vg_lite_color_key4_t structure#
The priority order is: color_key_0 > color_key_1 > color_key_2 > color_key_3. (from April 2022)
Used in blit function: vg_lite_set_color_key
vg_lite_color_key4_t members |
Type |
Description |
|---|---|---|
|
high_rgb_0, low_rgb_0, alpha_0, enable_0 |
|
|
high_rgb_1, low_rgb_1, alpha_1, enable_1 |
|
|
high_rgb_2, low_rgb_2, alpha_2, enable_2 |
|
|
high_rgb_3, low_rgb_3, alpha_3, enable_3 |
Parent topic:Blit structures
vg_lite_matrix_t structure#
Defined under the “Matrix control structures” section (see vg_lite_matrix_t structure).
Parent topic:Blit structures
vg_lite_path_t structure#
Defined under the “Vector path structures” section (see vg_lite_path_t structure).
Parent topic:Blit structures
vg_lite_rectangle_t structure#
This structure defines a rectangle by using coordinates.
Used in blit function: vg_lite_clear.
vg_lite_rectangle_t member |
Type |
Description |
|---|---|---|
|
vg_lite_int32_t |
X origin of rectangle, left coordinate in pixels |
|
vg_lite_int32_t |
Y origin of rectangle, top coordinate in pixels |
|
vg_lite_int32_t |
X Width of rectangle in pixels |
|
vg_lite_int32_t |
Y Height of rectangle in pixels |
Parent topic:Blit structures
vg_lite_point_t structure#
This structure defines a 2D point (from March 2021).
Used in structure: vg_lite_point4_t.
vg_lite_point_t member |
Type |
Description |
|---|---|---|
X |
vg_lite_int32_t |
X value of coordinate |
Y |
vg_lite_int32_t |
Y value of coordinate |
Parent topic:Blit structures
vg_lite_point4_t structure#
This structure defines four 2D points that form a polygon. The points are defined by structure vg_lite_point_t. (from March 2021)
vg_lite_point4_t member |
Type |
Description |
|---|---|---|
|
vg_lite_int32_t each |
a set of four points |
Parent topic:Blit structures
vg_lite_float_point_t structure#
This structure defines a 2D float point (from March 2024).
Used in structure: vg_lite_float_point4_t.
vg_lite_float_point_t members |
Type |
Description |
|---|---|---|
x |
vg_lite_float_t |
X value of coordinate |
y |
vg_lite_float_t |
Y value of coordinate |
Parent topic:Blit structures
vg_lite_float_point4_t structure#
This structure defines four 2D float points that form a polygon. The points are defined by structure vg_lite_float_point_t. (from March 2024)
Used in blit function: vg_lite_get_transform_matrix.
vg_lite_float_point4_t members |
Type |
Description |
|---|---|---|
vg_lite_float_point[4] |
vg_lite_float_t each |
a set of four points |
Parent topic:Blit structures
Parent topic:Blits for compositing and blending