MCUXpresso SDK Documentation

Bug fixes and/or feature enhancements#

Firmware version: From 16.91.21.p64.1 to 16.91.21.p82#

Component

Description

Wi-Fi

  • WPA3-R3 enabled APUT beacons does not have RSNXE when configured in H2E mode
  • Associated event is received even when connecting using wrong password
  • WFA APUT Low iperf TCP/UDP Tx throughput with Realtek station

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p82 to 16.91.21.p91.6#

Component

Description

Wi-Fi

  • In wrong password scenario, After updating new password the phone is not able to connect with DUTAP

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p91.6 to 16.91.21.p124#

Component

Description

Wi-Fi

  • Cloud keep alive packets not seen after DUT enters host sleep. DUT is sending QOS null packets even in host sleep

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p124 to 16.91.21.p133#

Component

Description

Wi-Fi

  • Samsung S24 Ultra and Google Pixel 7 mobiles having Android 14 are not able connect to the DUTAP with WPA3 SAE security.

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p133 to 16.91.21.p142.5#

Component

Description

Wi-Fi

  • Fails to encrypt and decrypt data with ccmp 128 and 256 using CLI crypto commands.

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p142.5 to 16.91.21.p149.2#

Component

Description

Wi-Fi

  • DUTSTA does not associate to hidden SSID beaconing in DFS channel.

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p149.2 to 16.92.21.p151.7#

Component

Description

Wi-Fi

  • Getting low TCP/UDP TP in DUT-AP 11ac-vht80 mode after hard-reset or wlan-reset.

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.91.21.p149.2 to 16.92.21.p151.7#

Component

Description

Wi-Fi

  • Getting low TCP/UDP TP in DUT-AP 11ac-vht80 mode after hard-reset or wlan-reset.

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.92.21.p151.7 to 16.92.21.p153.5#

Component

Description

Wi-Fi

  • Added P2P Persistance and P2P Invitation

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.92.21.p153.5 to 16.92.21.p153.6#

Component

Description

Wi-Fi

Enabled mbedtls 3.x

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.92.21.p153.6 to 16.92.21.p153.9#

Component

Description

Wi-Fi

  • Enabled mbedtls 3.x
  • The HT/VHT Wi-Fi capabilities are not being properly configured when the Device Under Test (DUT) initiates operation as a P2P Group Owner (P2P-GO).
  • Resolved RT685 Wi-Fi EAP-TLS crash caused by expired certificates

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.92.21.p153.9 to 16.92.21.p155.2#

Component

Description

Wi-Fi

  • Enabled mbedtls 3.x

Parent topic:Bug fixes and/or feature enhancements

Firmware version: From 16.92.21.p155.2 to 16.92.21.p156.1#

Component

Description

Wi-Fi

Fixed roaming failure (RRM-NEIGHBOR-REP-REQUEST-FAILED) when DUT roams between APs on different 5 GHz channels on i.MXRT685 platform.

Bluetooth

Fixed same EN_RAND value being generated on every AES-CCM encryption, causing predictable random number in BT pairing.

Parent topic:Bug fixes and/or feature enhancements

Parent topic:88W8987 release notes