Host API Python Bindings#
Prerequisites#
Python 3.10.x/32b is necessary to run the Python bindings. The bindings use the Host API C libraries. On Linux and OS X operating systems, these are called from the installation location which is /usr/local/lib, while on Windows OS the library file is loaded in <Python Install Directory>\DLLs.
Platform setup#
To run scripts from the command line, the PYTHONPATH must be set accordingly, so that the interpreter can find the imported modules.
Linux OS
Adding the source folder to the PYTHONPATH can be done by editing ~/.bashrc and adding the following line:
export PYTHONPATH=\$PYTHONPATH:/home/.../hsdk-python/src
Most of the Python scripts operate on boards connected on a serial bus and superuser privileges must be employed to access the ports. After running a command prefixed with sudo, the environment paths become those of root, so the locally set PYTHONPATH is not visible anymore. That is why /etc/sudoers is modified to keep the environment variable when changing user.
Edit /etc/sudoers with your favorite text editor. Modify:
Defaults env_reset -> Defaults env_keep="PYTHONPATH"
As an alternative to avoid modifying the :sudoers file, the PYTHONPATH can be adjusted programmatically, as in the example below:
import sys
if sys.platform.startswith('linux'):
sys.path.append('/home/user/hsdk-python/src')
Windows OS
Add the source folder to the PYTHONPATH by following these steps:
Navigate to My Computer > Properties > Advanced System Settings > Environment Variables > System Variables.
Modify existing or create new variable named PYTHONPATH, with the absolute path of
tools\wireless\host_sdk\hsdk-python\src.
Directory Tree#
lib Compiled host SDK libraries for Windows.
├── README.md
├── x64
│ └── HSDK.dll
└── x86
└── HSDK.dll
src
├── com
│ ├── nxp
│ │ ├── wireless_connectivity
│ │ │ ├── commands
│ │ │ │ ├── ble Generated files for Bluetooth LE support.
│ │ │ │ │ ├── ble_sig_defines.py
│ │ │ │ │ ├── enums.py
│ │ │ │ │ ├── events.py
│ │ │ │ │ ├── frames.py
│ │ │ │ │ ├── gatt_database_dynamic.py
│ │ │ │ │ ├── heart_rate_interface.py
│ │ │ │ │ ├── __init__.py
│ │ │ │ │ ├── operations.py
│ │ │ │ │ ├── spec.py
│ │ │ │ │ └── sync_requests.py
│ │ │ │ ├── comm.py
│ │ │ │ ├── firmware Generated files for OTA/FSCI bootloader support.
│ │ │ │ │ ├── enums.py
│ │ │ │ │ ├── events.py
│ │ │ │ │ ├── frames.py
│ │ │ │ │ ├── __init__.py
│ │ │ │ │ ├── operations.py
│ │ │ │ │ ├── spec.py
│ │ │ │ │ └── sync_requests.py
│ │ │ │ ├── fsci_data_packet.py
│ │ │ │ ├── fsci_frame_description.py
│ │ │ │ ├── fsci_operation.py
│ │ │ │ ├── fsci_parameter.py
│ │ │ │ └── __init__.py
│ │ │ ├── hsdk
│ │ │ │ ├── CFsciLibrary.py
│ | | │ ├── config.py Configuration file for the Python Host SDK subsystem.
│ │ │ │ ├── CUartLibrary.py
│ │ │ │ ├── device
│ │ │ │ │ ├── device_manager.py
│ │ │ │ │ ├── __init__.py
│ │ │ │ │ └── physical_device.py
│ │ │ │ ├── framing
│ │ │ │ │ ├── fsci_command.py
│ │ │ │ │ ├── fsci_framer.py
│ │ │ │ │ └── __init__.py
│ │ │ │ ├── __init__.py
│ │ │ │ ├── library_loader.py
│ │ │ │ ├── ota_server.py
│ │ │ │ ├── singleton.py
│ │ │ │ ├── sniffer.py
│ │ │ │ └── utils.py
│ │ │ ├── __init__.py
│ │ │ └── test Test and proof of concept scripts.
│ │ │ ├── hrs.py Script implementing a Bluetooth LE Heart Sensor profile .
│ │ │ └── __init__.py
│ │ └── __init__.py
│ └── __init__.py
└── __init__.py
Functional description#
The interaction between Python and the C libraries is made by the ctypes module. Ctypes provides C compatible data types, and allows calling functions in DLLs or shared libraries. It can be used to wrap these libraries in pure Python. Because the use of shared libraries is a requirement, the LIB_OPTION variable must remain set on “dynamic” in hsdk/Makefile. Ctypes made into mainline Python starting with version 2.5.
The Python Bindings expose Bluetooth LE familiar API in the com.nxp.wireless_connectivity.commands package. Such a package contains the following modules:
bluetooth le
├── enums.py – Classes that resemble enums, constants are generated here.
├── events.py – Observer classes that can build an object from a byte array and deliver it to the user.
├── frames.py – Classes that map on Bluetooth LE/Firmware FSCI messages.
├── operations.py – Each Operation class encapsulates a request and one or multiple events that are to be generated by the request.
├── spec.py – This file describes the name, size, order and relationship between the command parameters.
└── sync_requests.py – Each Synchronous Request is a method which sends a request and returns the triggered event.
Tests and examples are placed in the package com.nxp.wireless_connectivity.test.
Bluetooth LE Heart Rate Service use case#
The Heart Rate Service is presented as use case for using the API of a Bluetooth LE black box, located in the example hsdk-python/src/com/nxp/wireless_connectivity/test/hrs.py.
The example populates the GATT Database dynamically with the GATT, GAP, heart rate, battery and device information services. It then configures the Bluetooth LE stack and starts advertising. There are also two connect and disconnect observers to handle specific events.
The user needs to connect to the Bluetooth LE or hybrid black box through a serial bus port that is passed as a command line argument, for example, /dev/ttyACM0.
# python hrs.py -h
usage: hrs.py [-h] [-p] serial_port
Bluetooth LE demo app which implements a ble_fsci_heart_rate_sensor.
positional arguments:
serial_port Kinetis-W system device node.
optional arguments:
-h, --help show this help message and exit
-p, --pair Use pairing
It is important to first execute a CPU reset request to the Bluetooth LE black box before performing any other configuration to reset the Buetooth LE stack. This is done by the following command:
FSCICPUReset(serial_port, protocol=Protocol.BLE)
User sync request example
It is recommended for the user to access the Bluetooth LE API through sync requests. GATTDBDynamicAddCharacteristicDeclarationAndValue API is used as an example:
def gattdb_dynamic_add_cdv(self, char_uuid, char_prop, maxval_len, initval, val_perm):
'''
Declare a characteristic and assign it a value.
@param char_uuid: UUID of the characteristic
@param char_prop: properties of the characteristic
@param maxval_len: maximum length of the value
@param initval: initial value
@param val_perm: access permissions on the value
@return: handle of the characteristic
'''
ind = GATTDBDynamicAddCharacteristicDeclarationAndValue(
self.serial_port,
UuidType=UuidType.Uuid16Bits,
Uuid=char_uuid,
CharacteristicProperties=char_prop,
MaxValueLength=maxval_len,
InitialValueLength=len(initval),
InitialValue=initval,
ValueAccessPermissions=val_perm,
protocol=self.protocol
)
if ind is None:
return self.gattdb_dynamic_add_cdv(char_uuid, char_prop, maxval_len, initval, val_perm)
print '\tCharacteristic Handle for UUID 0x%04X ->' % char_uuid, ind.CharacteristicHandle
self.handles[char_uuid] = ind.CharacteristicHandle
return ind.CharacteristicHandle
Sync request internal implementation
As an example, for the GATTDBDynamicAddCharacteristicDeclarationAndValue API, the command is executed through a synchronous request. The sync request code creates an object of the following class:
class GATTDBDynamicAddCharacteristicDeclarationAndValueRequest(object):
def __init__(self,
UuidType=GATTDBDynamicAddCharacteristicDeclarationAndValueRequestUuidType.Uuid16Bits, Uuid=[],
CharacteristicProperties=GATTDBDynamicAddCharacteristicDeclarationAndValueRequestCharacteristicProperties.gNone_c,
MaxValueLength=bytearray(2), InitialValueLength=bytearray(2), InitialValue=[],
ValueAccessPermissions=GATTDBDynamicAddCharacteristicDeclarationAndValueRequestValueAccessPermissions.gPermissionNone_c):
'''
@param UuidType: UUID type
@param Uuid: UUID value
@param CharacteristicProperties: Characteristic properties
@param MaxValueLength: If the Characteristic Value length is variable, this is the maximum length; for fixed lengths this must be set to 0
@param InitialValueLength: Value length at initialization; remains fixed if maxValueLength is set to 0, otherwise cannot be greater than maxValueLength
@param InitialValue: Contains the initial value of the Characteristic
@param ValueAccessPermissions: Access permissions for the value attribute
'''
self.UuidType = UuidType
self.Uuid = Uuid
self.CharacteristicProperties = CharacteristicProperties
self.MaxValueLength = MaxValueLength
self.InitialValueLength = InitialValueLength
self.InitialValue = InitialValue
self.ValueAccessPermissions = ValueAccessPermissions
An operation is represented by an object of the following class:
class GATTDBDynamicAddCharacteristicDescriptorOperation(FsciOperation):
def subscribeToEvents(self):
self.spec = Spec.GATTDBDynamicAddCharacteristicDescriptorRequestFrame
self.observers =[GATTDBDynamicAddCharacteristicDescriptorIndicationObserver('GATTDBDynamicAddCharacteristicDescriptorIndication'), ]
super(GATTDBDynamicAddCharacteristicDescriptorOperation, self).subscribeToEvents()
The Spec object is initialized and set to zero in the FSCI packet any parameter not passed through the object of a class, depending on its length. Also, when defining such an object, the parameters may take simple integer, boolean or even list values instead of byte arrays, the values are serialized as a byte stream.
The observer is an object of the following class:
class GATTDBDynamicAddCharacteristicDeclarationAndValueIndicationObserver(Observer):
opGroup = Spec.GATTDBDynamicAddCharacteristicDeclarationAndValueIndicationFrame.opGroup
opCode = Spec.GATTDBDynamicAddCharacteristicDeclarationAndValueIndicationFrame.opCode
@overrides(Observer)
def observeEvent(self, framer, event, callback, sync_request):
# Call super, print common information
Observer.observeEvent(self, framer, event, callback, sync_request)
#Get payload
fsciFrame = cast(event, POINTER(FsciFrame))
data = cast(fsciFrame.contents.data, POINTER(fsciFrame.contents.length * c_uint8))
packet = Spec.GATTDBDynamicAddCharacteristicDeclarationAndValueIndicationFrame.getFsciPacketFromByteArray(data.contents, fsciFrame.contents.length)
# Create frame object
frame = GATTDBDynamicAddCharacteristicDeclarationAndValueIndication()
frame.CharacteristicHandle = packet.getParamValueAsNumber("CharacteristicHandle")
framer.event_queue.put(frame) if sync_request else None
if callback is not None:
callback(frame)
else:
print_event(self.deviceName, frame)
fsciLibrary.DestroyFSCIFrame(event)
The status of the request is printed at the console by the following general status handler:
def subscribe_to_async_ble_events_from(device, ack_policy=FsciAckPolicy.GLOBAL):
ble_events = [
L2CAPConfirmObserver('L2CAPConfirm'),
GAPConfirmObserver('GAPConfirm'),
GATTConfirmObserver('GATTConfirm'),
GATTDBConfirmObserver('GATTDBConfirm'),
GAPGenericEventInitializationCompleteIndicationObserver('GAPGenericEventInitializationCompleteIndication'),
GAPAdvertisingEventCommandFailedIndicationObserver('GAPAdvertisingEventCommandFailedIndication'),
GATTServerErrorIndicationObserver('GATTServerErrorIndication'),
GATTServerCharacteristicCccdWrittenIndicationObserver('GATTServerCharacteristicCccdWrittenIndication')
]
for ble_event in ble_events:
FsciFramer(device, FsciAckPolicy.GLOBAL, Protocol.BLE, Baudrate.BR115200).addObserver(ble_event)
Connect and disconnect observers
The following code adds observers for the connect and disconnect events in the user class:
class BLEDevice(object):
'''
Class which defines the actions performed on a generic Bluetooth LE device.
Services implemented: GATT, GAP, Device Info.
'''
self.framer.addObserver(
GAPConnectionEventConnectedIndicationObserver('GAPConnectionEventConnectedIndication'),
self.cb_gap_conn_event_connected_cb)
self.framer.addObserver(GAPConnectionEventDisconnectedIndicationObserver('GAPConnectionEventDisconnectedIndication'),
self.cb_gap_conn_event_disconnected_cb)
where the callbacks are:
def cb_gap_conn_event_connected_cb(self, event):
'''
Callback executed when a smartphone connects to this device.
@param event: GAPConnectionEventConnectedIndication
'''
print_event(self.serial_port, event)
self.client_device_id = event.DeviceId
self.gap_event_connected.set()
def cb_gap_conn_event_disconnected_cb(self, event):
'''
Callback executed when a smartphone disconnects from this device.
@param event: GAPConnectionEventdisConnectedIndication
'''
print_event(self.serial_port, event)
self.gap_event_connected.clear()
From an Android™ or iOS-based smartphone, the user can use the Bluetooth LE Toolbox application in the Heart Rate profile. Random heart rate measurements in the range 60-100 are displayed every second, while battery values change every 10 seconds.
Parent topic: Bluetooth Low Energy Host Stack FSCI Application Programming