MCUXpresso SDK Documentation

MCUXpresso SDK : audio-voice-components#

Overview#

This repository is for MCUXpresso SDK audio-voice-components middleware delivery and it contains the components officially provided in NXP MCUXpresso SDK. This repository is part of the MCUXpresso SDK overall delivery which is composed of several sub-repositories/projects. Navigate to the top/parent repository (mcuxsdk-manifests) for the complete delivery of MCUXpresso SDK.

Documentation#

Overall details can be reviewed here: MCUXpresso SDK Online Documentation

Visit Audio Voice Components - Documentation to review details on the contents in this sub-repo.

Setup#

Instructions on how to install the MCUXpresso SDK provided from GitHub via west manifest Getting Started with SDK - Detailed Installation Instructions

Contribution#

Contributions are not currently accepted. Guidelines to contribute will be posted in the future.


Overview#

This repository allows users to add additional functionality to the Maestro Audio framework. This structure is designed for integration with Maestro and is not intended for standalone use. For information on the use of individual components, please refer to the Maestro programmer’s guide.

This repository acts as Zephyr module, to be able to use these libraries in Zephyr build system.

Content#

  • asrc - Libraries and public files of Asynchronous Sample Rate Converter, version 1.0.0

  • ssrc - Libraries and public files of Synchronous Sample Rate Converter, version 1.0.0

  • opus - Source files of Opus decoder and encoder, version 1.3.1

  • opusfile - Source files for Opus streams in the Ogg container, version 0.12

  • ogg - Source files of Ogg container, version 1.3.5

  • decoders - Libraries and public files of following audio decoders:

    • aac - AAC decoder, version 1.0.0

    • flac - FLAC decoder, version 1.0.0

    • mp3 - MP3 decoder, version 1.0.0

    • wav - WAV decoder, version 1.0.0

  • zephyr/ - Files allowing usage of the libraries in Zephyr build

Following table contains information about libraries and source files availability:

Processor Toolchain Source files
Cortex-M7(F) Cortex-M33(F) ARM GCC IAR
ASRC Yes X
Yes X X
SSRC Yes Yes Yes Yes X
Opus X X X X Yes
Opus File X X X X Yes
Ogg Container X X X X Yes
AAC Yes Yes Yes X X
FLAC Yes Yes Yes Yes X
MP3 Yes Yes Yes Yes X
WAV Yes Yes Yes Yes X

Asynchronous Sample Rate Converter#

The Asynchronous Sample Rate Converter (ASRC) software module compensates the drift between two mono audio signals. This is not a frequency converter and so the nominal signal frequency is the same before and after the ASRC. More details about ASRC are available in the User Guide, which is located in asrc\doc\.

Synchronous Sample Rate Converter#

The Synchronous Sample Rate Converter (SSRC) software module converts an audio signal (mono or stereo) with a certain sampling frequency to an audio signal with another sampling frequency. More details about SSRC are available in the User Guide.

Opus#

For Opus decoder and encoder documentation please see following link: opus.

Opus File#

The Opus File provides a API for decoding and basic manipulation of Opus streams in Ogg container and depends on Opus and Ogg libraries. For Opus File documentation please see following link: opusfile.

Ogg Container#

For Ogg container documentation please see following link: ogg.

Decoders#

Each decoder contains libraries for supported processor and toolchain (see table above), corresponding Public API file and documentation folder.

AAC#

For decoder features please see aacdec, for API Usage please see aacd_ug.

FLAC#

For decoder features please see flacdec, for API Usage please see flacd_ug.

MP3#

For decoder features please see mp3dec, for API Usage please see mp3d_ug.

WAV#

For decoder features please see wavdec, for API Usage please see wavd_ug.

Zephyr build#

To add library into the Zephyr build, add CONFIG_NXP_AUDIO_VOICE_COMPONENTS_* for specific libraries into your prj.conf. For all configuration options, see zephyr/Kconfig.

List of supported libraries in Zephyr:

  • Decoders:

    • AAC

    • FLAC

    • MP3

    • FLAC

    • OPUS

  • Encoders

    • OPUS