lvgl_guider# Overview# This project is used to work with LittleVGL GUI Guider. The GUI Guider generated code is placed in the folder “generated”. The example generated code shows a rectangle in the panel, drag it, then it will move in the screen. Supported Boards# EVKB-IMXRT1050 MIMXRT1060-EVKB MIMXRT1170-EVKB MIMXRT1060-EVKC EVK-MIMXRT1010 EVK-MIMXRT1015 EVK-MIMXRT1020 MIMXRT1024-EVK MIMXRT1040-EVK EVK-MIMXRT1064 MIMXRT1160-EVK EVK-MIMXRT595 EVK-MIMXRT685 FRDM-IMXRT700 FRDM-K22F FRDM-MCXA156 FRDM-MCXN236 FRDM-MCXN947 FRDM-RW612 LPCXpresso51U68 LPCXpresso54628 LPCXpresso54S018 LPCXpresso54S018M LPCXpresso55S06 LPCXpresso55S16 LPCXpresso55S28 LPCXpresso55S36 LPCXpresso55S69 MCX-N5XX-EVK MCX-N9XX-EVK MIMXRT685-AUD-EVK MIMXRT700-EVK RD-RW612-BGA FRDM-MCXA266 FRDM-MCXA366 FRDM-MCXA287 FRDM-MCXA577