MCUXpresso SDK Documentation

ecat_digital_io#

Overview#

This example demonstrates how to develop a remote IO device based on Slave Stack Code(SSC).

This remote IO device only supports SM-Synchron mode for DC operation, and implements one Input channel and one Output channel:

Output channel: connected with the LED and used to control this LED.

Input channel: used to read the LED current status. 

Note that the demo CAN NOT be built directly. Please see the “Prepare the Demo” section for more details.

Running the demo#

When the example is running, the serial port will output:

   Start the SSC digital_io example...

After the PLC program started, the LED starts to blink with 0.5Hz frequency.

NOTE: refer to the User Guide for the details of how to setup the PLC project on TwinCAT3.

TwinCAT Setup#

To demonstrate this IO example, TwinCAT is used as the EtherCAT MainDevice.

Supported Boards#