dev_composite_hid_mouse_hid_keyboard
Overview
The application is a simple demonstration program based on the MCUXpresso SDK. The application is enumerated as HID-compliant mouse and keyboard devices.
System Requirement
Hardware requirements
- Mini/micro USB cable 
- USB A to micro AB cable 
- Hardware (Tower module/base board, and so on) for a specific device 
- Personal Computer (PC) 
Software requirements
- The project files for lite version examples are in: 
 <MCUXpresso_SDK_Install>/boards/- /usb_examples/usb_device_composite_hid_mouse_hid_keyboard_lite/ - / - . 
 For non-lite version example, the files are in:
 <MCUXpresso_SDK_Install>/boards/- /usb_examples/usb_device_composite_hid_mouse_hid_keyboard/ - / - . 
The
is Bare Metal or FreeRTOS OS. 
Getting Started
Hardware Settings
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
- Download the program to the target board. 
- Connect the target board to the external power source (the example is self-powered). 
- Power off the target board. And then power on again. 
- Connect a USB cable between the PC and the USB device port of the board. 
For detailed instructions, see the appropriate board User’s Guide.
Run the example
- Plug in the device, which is running the composite example, into PC. An HID-compliant mouse and a keyboard are enumerated in the Device Manager. 
- For the HID mouse, the mouse arrow moving on the PC screen in the rectangular rotation.\n 
- For the HID keyboard, see the screen while scrolling up and down. 
*/
Supported Boards
- MIMXRT1170-EVKB 
- FRDM-K22F 
- LPCXpresso55S69 
- EVK-MIMXRT1064 
- FRDM-MCXA153 
- MIMXRT685-AUD-EVK 
- LPCXpresso51U68 
- LPCXpresso54S018 
- LPCXpresso54S018M 
- MIMXRT1060-EVKB 
- EVK-MIMXRT1010 
- MIMXRT1040-EVK 
- FRDM-MCXN947 
- MIMXRT1024-EVK 
- LPCXpresso55S28 
- LPCXpresso54628 
- LPCXpresso55S36 
- MCX-N5XX-EVK 
- MIMXRT1060-EVKC 
- MIMXRT1160-EVK 
- MIMXRT1180-EVK 
- EVK-MIMXRT1020 
- MIMXRT700-EVK 
- FRDM-MCXA156 
- EVK-MIMXRT595 
- EVK-MIMXRT685 
- MCX-N9XX-EVK 
- EVKB-IMXRT1050 
- RD-RW612-BGA 
- FRDM-K32L3A6 
- EVK-MIMXRT1015 
- FRDM-MCXN236 
- FRDM-RW612