Hardware requirements
- Mini/micro USB cable 
- EVKB-IMXRT1050 board 
- Personal Computer 
Board settings
No special settings are required.
Prepare the Demo
- Connect a USB cable between the host PC and the OpenSDA USB port on the target board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. 
Note
- This demo will access GPIO DR_SET/DR_CLEAR registers which is only available on A1 silicon (MIMXRT105xxxxxB). 
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
CMP interrupt Example
Then change CMP analog input, and watch the change of LED. - CMP1_IN0 (J23-5) connected to VCC =3.3V (J24-8): USER LED on - CMP1_IN0 (J23-5) connected to GND (J24-7): USER LED off