Hardware requirements
- Micro USB cable 
- MIMXRT1180-EVK board 
- Personal Computer 
Board settings
No special settings are required.
Prepare the Demo
- Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board. 
- Connect a micro USB cable between the host PC and the J17 USB port on the cpu board. 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Launch the debugger in your IDE to begin running the example. 
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TPM example to simulate a timer
You will see a "-" or "|" in terminal every 1 second:
-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-|-