Hardware requirements
- Micro USB cable 
- EVK-MIMXRT595 board 
- Personal Computer 
Board settings
Prepare the Demo
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board 
- Open a serial terminal with the following settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Launch the debugger in your IDE to begin running the demo. 
Running the demo
The log below shows the output of the shell demo in the terminal window:
SHELL build: Sep 27 2020
Copyright  2020  NXP
LOG SHELL>> installbackend debugconsole
LOG SHELL>> log fatal
           0: FATAL log_main.c:83:This is "fatal" log message
LOG SHELL>> log error
           0: ERROR log_main.c:87:This is "error" log message
LOG SHELL>> log warning
           0: WARN  log_main.c:91:This is "warning" log message
LOG SHELL>> log info
           0: INFO  log_main.c:95:This is "info" log message
LOG SHELL>> log debug
           0: DEBUG log_main.c:99:This is "debug" log message
LOG SHELL>> log trace
           0: TRACE log_main.c:103:This is "trace" log message
LOG SHELL>> log test
           0: ERROR log_main.c:107:The input arguement "test" is not valid
LOG SHELL>> uninstallbackend debugconsole
LOG SHELL>> 
Note: The shell information “SHELL build: Sep 27 2020” may be different, which depends on the compile date.