MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • EVK-MIMXRT595 REV C1 board

  • Personal Computer

Board settings#

Make sure resistors R691~R697 are removed and resistors R611~R620,R660,R661,R698 are populated.

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

When the demo runs successfully, the log would be seen on the terminal like:

FATFS example to demonstrate how to use FATFS with MMC card.



Make file system......The time may be long if the card capacity is big.



Create directory......



Create a file in that directory......



List the file in that directory......

General file : F_1.DAT.



 Write/read file until encounters error......



Write to above created file.

Read from above created file.

Compare the read/write content.

The read/write content is consistent.



Input 'q' to quit read/write.

Input other char to read/write file again.