Hardware requirements
- Mini/micro USB cable 
- FRDM-K32L2A4S board 
- Personal Computer 
Board settings
No special is needed.
Prepare the Demo
- Connect a mini USB cable between the PC host and the OpenSDA USB port on the board. 
- Connect the analog signal source’s output to the input of used-defined comparator’s channel (defined as “DEMO_CMP_USER_CHANNEL” in source code.) 
- Open a serial terminal on PC for OpenSDA serial device with these settings: - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Reset the SoC and run the project. 
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
CMP interrupt Example.
Then change CMP analog input, and watch the change of LED. - CMP0_IN1 (Jump J1-11) connected to VCC=3.3V(Jump J3-8): LED RED on - CMP0_IN1 (Jump J1-11) connected to GND (Jump J2-14): LED RED off