Hardware requirements
Type-C USB cable
FRDM-MCXL255 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port (J16) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
Flash driver API tree demo application.
Initializing flash driver.
Flash init successfull!
Config flash memory access time.
PFlash Information:
kFLASH_PropertyPflashBlockBaseAddr = 0x0
kFLASH_PropertyPflashSectorSize = 8192
kFLASH_PropertyPflashTotalSize = 262144
kFLASH_PropertyPflashPageSize = 0x80
Erase a sector of flash
Calling flash_verify_erase_sector() API.
Successfully erased sector: 0x3c000 -> 0x3e000
Calling FLASH_Program() API.
Calling FLASH_VerifyProgram() API.
Successfully programmed and verified location: 0x3c000 -> 0x3c200
End of PFlash Example!