Hardware requirements
- Micro USB cable 
- LPCXpresso51U68 board 
- Personal Computer 
Board settings
Populate jumper JP3. Connect SPI5 pins to SPI3 pins:
Master - SPI5                 CONNECTS TO      Slave - SPI3
Pin Name   Board Location                      Pin Name  Board Location
MISO       J1 pin 11                           MISO      J4 pin 3
MOSI       J1 pin 13                           MOSI      J4 pin 2
SCK        J2 pin 8                            SCK       J4 pin 4
PCS2       J1 pin 15                           PCS2      J4 pin 7
Prepare the Demo
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board 
- Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number): - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Reset the SoC and run the project. 
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!