Hardware requirements
- Micro USB cable 
- LPCXpresso55S28 board 
- Personal Computer 
Board settings
    Master_board(SPI7)           Slave_board(SPI2)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       P17  pin 12         MISO      P18  pin 6
MOSI       P17  pin 10         MOSI      P18  pin 10
SCK        P17  pin 14         SCK       P18  pin 8
SSEL1      P17  pin 1          SSEL0     P17  pin 16
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
- Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board 
- Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number): - 115200 baud rate 
- 8 data bits 
- No parity 
- One stop bit 
- No flow control 
 
- Download the program to the target board. 
- Reset the SoC and run the project. 
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI one board interrupt example started!
SPI transfer finished!
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~